Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Battery Management ICs Forum Discussions

navya
Battery Management ICs
Dear team, i am using the relay driver ic with part number TLE75602 on Battery management system board,the board and relay driver ic input voltage is ... Show More
Translation_Bot
Battery Management ICs
1. This part of the application block diagram is not well understood, but simply understood as follows: when the input voltage is lower than the rated... Show More
Translation_Bot
Battery Management ICs
IR software configuration IRPS5401 chip, chip address i2c: 0x14, PMbus address: 0x44, offset address: +4, the problem is that the first time the conne... Show More
iCatlett
Battery Management ICs
Hello, I was a custom PCB that is based off of the REFWLCTX15WC1. The layout is different from the development board but the circuitry is the exact sa... Show More
yuyuyu
Battery Management ICs
你好, 我想了解以下内容: 1.TLE9012DQU使用8串电池采样应该怎么连接,是将G8~U12短接吗? 2.与MCU通讯是将GPIO0 /UART_LS接到MCU的UART-RX,将GPIO1 /UART_HS接到TX吗?不使用链式结构 IFL_L、IFL_H、IFH_H、IFH_L这四个引脚该... Show More
Sudo_Darshan
Battery Management ICs

Hi Infinineon team , can you please provide an updated data sheet for TLE75008 , which reads  ChipID'S

 

thang
Battery Management ICs
Hello,   I am looking for a battery management system for our lead acid batteries. The total voltage of battery rack is 300V. Do you have a proposal o... Show More
lachavusache
Battery Management ICs
Hi everyone,  I am trying to read the battery data from TLE9012DQU without using the default hex file. I have written the following function to send c... Show More
Anaconda91
Battery Management ICs
C/C++ drivers
solved msg Solved
Good day!  Is there any information about c/c++ drivers fr IC`s  TLE9012DQU & APD 2ED4820-EM? Best regards! Show More
YuanChangSoo
Battery Management ICs

Any replacement for TLE9261QX ?

The part status show "Discontinue". 

Forum Information

Battery Management ICs

Infineon's TLE9012DQU is a multi channel battery monitoring and balancing IC for various lithium-ion battery applications, with integral functions like voltage and temperature measurement, cell balancing, and isolated communication with the main battery controller, including self-diagnosis features. The TLE9015DQU iso UART Transceiver IC is used in battery systems for enabling the communication between the main microcontroller and multiple TLE9012DQU units in a daisy-chain configuration. This forum welcomes discussions, queries, and insights on battery management systems and devices.