Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Battery Management ICs Forum Discussions

iCatlett
Battery Management ICs
Hello, I was a custom PCB that is based off of the REFWLCTX15WC1. The layout is different from the development board but the circuitry is the exact sa... Show More
yuyuyu
Battery Management ICs
你好, 我想了解以下内容: 1.TLE9012DQU使用8串电池采样应该怎么连接,是将G8~U12短接吗? 2.与MCU通讯是将GPIO0 /UART_LS接到MCU的UART-RX,将GPIO1 /UART_HS接到TX吗?不使用链式结构 IFL_L、IFL_H、IFH_H、IFH_L这四个引脚该... Show More
lachavusache
Battery Management ICs
Hi everyone,  I am trying to read the battery data from TLE9012DQU without using the default hex file. I have written the following function to send c... Show More
Anaconda91
Battery Management ICs
C/C++ drivers
solved msg Solved
Good day!  Is there any information about c/c++ drivers fr IC`s  TLE9012DQU & APD 2ED4820-EM? Best regards! Show More
YuanChangSoo
Battery Management ICs

Any replacement for TLE9261QX ?

The part status show "Discontinue". 

AriesLhc
Battery Management ICs
How to solve the problem of severe heating of the driving chip when driving a PWM signal of 200KHZ? Currently, air-cooled cooling is used for heat dis... Show More
Translation_Bot
Battery Management ICs
I would like to know why the BTS50085 outputs no output after the capacitive load is increased, and how to solve this problem. Show More
che
Battery Management ICs
Hi Expertises, In TLE9012 DQU chapter 17 mentioned that "Cell voltage supervision warning flags CELL_UV_DAC_COMP" and "Cell voltage supervision warnin... Show More
Translation_Bot
Battery Management ICs
ICE3PCS03G
solved msg Solved
ICE3PCS03G PFC management chip boost voltage does not reach the ideal value of the problem: BOOST inductance of about 500UH, capacitance 2000uh curren... Show More
Coolllama
Battery Management ICs
Hi, Is any AURIX TC3xx TFT available and compatible with TLE9015DQU_TRX_BRG and TLE9012DQU_DTR_BMS2 evaluation boards? Regards, Show More
Forum Information

Battery Management ICs

Infineon's TLE9012DQU is a multi channel battery monitoring and balancing IC for various lithium-ion battery applications, with integral functions like voltage and temperature measurement, cell balancing, and isolated communication with the main battery controller, including self-diagnosis features. The TLE9015DQU iso UART Transceiver IC is used in battery systems for enabling the communication between the main microcontroller and multiple TLE9012DQU units in a daisy-chain configuration. This forum welcomes discussions, queries, and insights on battery management systems and devices.