Applications Forum Discussions
Browse the Community
Adapters and Chargers
This forum discusses Adapter and Charger applications based on Infineon products. This includes USB-C chargers and adapters, Automotive USB-C charging, and Battery chargers.
Featured Discussions
Dear experts
I already use Infineon solution to design PD3.1 application.
and I have some questions about design document, please give me some suggestions, thanks.
1. how do you know the resonant period is Tr/2? could you please explain it more detail?
2. When should the secondary-side MOSFET be turned off, and how can this objective be achieved using open-loop control in SIMPLIS, I would like to use SIMPLIS to know the operation of AHB CRM mode, but it seems you don't have any simulation file in the website. if I use diode in the secondary is it ok?
3.Why is the waveform at the red-circled region different in these two images?
4. How to determine the dead time and the value of capacitor Cr?
5. How to optimize the CM noise in this topology? I want to modify it from the transformer side.
Show Less
Dear experts
I already use Infineon solution to design PD3.1 application.
and I have some questions about design document, please give me some suggestions, thanks.
1. how do you know the resonant period is Tr/2? could you please explain it more detail?
2. When should the secondary-side MOSFET be turned off, and how can this objective be achieved using open-loop control in SIMPLIS, I would like to use SIMPLIS to know the operation of AHB CRM mode, but it seems you don't have any simulation file in the website. if I use diode in the secondary is it ok?
3.Why is the waveform at the red-circled region different in these two images?
4. How to determine the dead time and the value of capacitor Cr?
5. How to optimize the CM noise in this topology? I want to modify it from the transformer side.
Show Less
Hi
Myself : Nihal khan
In infineon code for PFC_Stage 3.3KW on board charger there is Ntc lookup table form where we are selecting the temperature based on the index value. i have doubt in calculation of ntc lookup table
pls share the the specification of NTC which is used in PFC_Stage 3.3KW on board charger and also the method or equations to calculate the ntc lookup table
Show LessIs there any solution for Phase Shedding in Multiphase Boost PFC using UCC28070 Controller?
Recently we need to confirm when ICE2QR1765's each pin short to each other or short to GND or short to VCC. While do not know detail design, so can you support us to analysis it ? Hope to receive your professional help~
Show Less
Hi all,
I am trying to understand why 75V Zener's are connected in PFC CT circuits, what's the reason of so high voltage rating. As Voltages across CT's secondary terminals would be in milli Volts.
I am attaching Circuit diagram for reference.
P.S: - the two signals PCS and NCS goes to Opam for control.
regards,
Show LessHi all,
I have been working on 2kW Charger board by Infineon "48 V lead-acid/Li-ion battery charger; AN_PL52_1903_161642 ", I have observed a very high current ripple at output, almost 20% at various load conditions and ripple frequency is 100Hz. Also tried increasing output inductor value by twice than what is recommended, but still issue persists, can anyone suggest ways to suppress high ripple.
Thank You,
Show LessDear IFXer,
1. ICE2QR4780G during operation, if CS fail(open and short), what will happen?
2. ICE2QR4780G has min. and max. switch frequency limitation?
3. ICE2QR4780G PWM's max on time is 30us, what is the switch frequency condition? and if Fs is 130kHz, the Duty exceeded 100%?
Show LessHi
I had bought one XDPS2201 65W EVM and dp Interface board GEN 2 from Mouser. I had installed the .dp Vision software on my PC, but it didn't work. It seems I need to install the add-on package which can't be found in the website.
Is it possible to provide the link or send the file to my email?
Show Less