AnyCloud SDK

cancel
Showing results for 
Search instead for 
Did you mean: 
Ask a question

Recent discussions

Sort by:
rkcypress
AnyCloud SDK
I have created a cypress docker image which has all dependencies required to run my UI tests.However when I am running my image in GitLab pipeline it ... Show More
austin_h
AnyCloud SDK
Hi, Can AnyCloud SDK (MQTT sample code)connect to Google Cloud Platform?? I am confused after studied GCP IoT Core guide information. https://cloud.google.com/iot/docs/how-tos/getting-started... Show More
skruglewicz
AnyCloud SDK
I trying to connect to my my home router I follow the instructions on the GitHub readme.me I'm getting the following error: Function whd_wifi_join fai... Show More
markgsaunders
AnyCloud SDK
We have discovered a problem with the lwip library in ModusToolbox 2.0, 2.1, 2.2 and 2.3. It occurs when creating a new Wi-Fi project or updating the ... Show More
lesmalave
AnyCloud SDK
I have not been able to fix the error "MQTT connection failed with error code 0x8060009 ..."I am implementing the mtb-example-anycloud-mqtt-client wit... Show More
AsRa_264661
AnyCloud SDK
Hi All,Checkout the recent BLE project with AnyCloud, Capsense to control the GoPro Hero 7 Camera.ThanksAshok Show More
raya_4824241
AnyCloud SDK
I am trying to run on a local network with an unsecure connection to an MQTT broker. The AnyCloud_MQTT_Client example fails to build if I change the M... Show More
LuisLop
AnyCloud SDK
Hello, guys! I am new in the world of BLE and I want to design a lite beacon device (with probably use of wifi on the future) based on the 4343W. For ... Show More
dk
AnyCloud SDK
Hi, I created a new app using the anycloud wifi server template, and flashed it on both of my dev boards. I only changed the SSID and password variabl... Show More
Frank-Lin
AnyCloud SDK
Hi,I am testing mqtt client and have some question.  1. How to get date time?        Using default code, i can connect to aws iot core. So it seems al... Show More