Has anyone successfully built and ran anycloud-ota-mqtt example on CY8CKIT-062-WIFI-BT Target? If so I need some help please.
I am getting a flash error...
I have
ModusToolbox
Version: 2.1.0
Build ID: 1905
Windows 7 Pro OS
Using PSOC 6 WIFI-BT Pioneer Kit
KitProg 3
Cypress Programmer 3.0.0 Build 463
Thanks
William
Solved! Go to Solution.
Dolt Dolt Dolt,
Well...
You caught me not reading and following directions...
But... Thank you so much! MuraliR_36 I thought I was doing something wrong, well I mean I thought something was wrong with my board.
I am glad I finally asked... No one was putting anything on the community so I figured I must be doing something wrong is that makes sense... LOL and I would figure it out...
I spent all day yesterday trying stufff...
I feel better
:thumbs up:
William
Hello WiWi_4702256
As mentioned in the the readme.md of GitHub - cypresssemiconductorco/mtb-example-anycloud-ota-mqtt: This code example demonstrates Over-t... The supported kits are PSoC 6 Wi-Fi BT Prototyping Kit and the PSoC 62S2 Wi-Fi BT Pioneer Kit. This is because the example is supported only on 2M flash devices. The error is expected since the PSoC 6 Wi-Fi BT Pioneer kit has just 1MB of flash which isn't sufficient to run the example.
Thanks
Dolt Dolt Dolt,
Well...
You caught me not reading and following directions...
But... Thank you so much! MuraliR_36 I thought I was doing something wrong, well I mean I thought something was wrong with my board.
I am glad I finally asked... No one was putting anything on the community so I figured I must be doing something wrong is that makes sense... LOL and I would figure it out...
I spent all day yesterday trying stufff...
I feel better
:thumbs up:
William