Angle (Magnetic sensor) Forum Discussions
text.format{('custom.tabs.no.results')}
Hello, Infineon team: We are currently using the TLE5012BE1000 for our application. Currently, the solution we are using is to communicate with the four SPI1 wires on the TC233 and the three SSC wires on the TLE5012BE1000. Currently, the main chip can read information such as angle values, turn values, angular speed values, etc. through SPI. I still want to read the chip's fault information. If so, can it be read through the SPI method and can it help solve the problem Thank you very much;
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E8%A7%92%E5%BA%A6-%E7%A3%81%E6%80%A7%E4%BC%A0%E6%84%9F%E5%99%A8/Read-the-fault-information-of-the-chip/td-p/684545
Show LessHi All,
Where can i find the IBIS model of TLE5012BE5000 for signal integrity analysis.
To be able to read the data from the register, the default value should be a forward increase of 0, and the flip starts and decreases at 7ffF, but even if you take the register value to 1, it's 128 °/s to calculate it. I don't think this value should be correct and I want to ask about the calculation method in this regard
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E8%A7%92%E5%BA%A6-%E7%A3%81%E6%80%A7%E4%BC%A0%E6%84%9F%E5%99%A8/TLE5012B-E1000%E7%AE%97%E5%87%BA%E7%9A%84%E8%A7%92%E9%80%9F%E5%BA%A6%E4%B8%8D%E6%AD%A3%E7%A1%AE/td-p/670961
Show LessHi experts,
I'm looking for something similar to the magnetic rotation angle sensor ams AS5600.
It produces an analog output similar to that of a potentiometer.
Does infineon have it?
thank you.
Show Less第一:对单个的TLV493D-A1B6,上电是否需要初始化。初始化过程中涉及到发送0x00h,进行复位并重置寄存器,此时iic的频率要求是多少?
第二,初始化时,发送是否一定要发送0xFFh,对探测器进行释放。
第三,对单个的TLV493D-A1B6进行操作,地址是否是确定的的,直接进行操作就行了,不需要初始化流程。
第三,能否提供一下,FPGA的代码,进行参考一下。
Show LessHello Infineon, as shown in the datasheet, user need to check safety word , include "CRC" , the CRC value of safety word will compare with the calculation value by uC, if no equal, CRC error.
I got a problem in our product, there is 1 pcs abnormal product and it will perform as "CRC" error, we never found this problem in our product and we also found the error seems like not relate operating conditions.
The question is : could you please provide some suggestion to figure out the problem?
Show Less
在使用TLE5012时,定位精度误差接近0.8度,在步进电机微步定位时,正向停止,反向走微步时会丢失6-8个脉冲,走到第8或者8步时,会把丢失的脉冲一次性发出来,各位大神是否有解决方案
为什么前雷达的国产化突破要比角雷达难?
麻烦工程师从技术难点等角度回答问题,并推荐英飞凌相关产品。非常感谢!
原帖链接如下:https://www.zhihu.com/question/610169734
Show LessHello,
We are using TLE4999C8 Hall Sensor, for our application we wanted to implement the Short Serial Message (SSM) feature.
We are able to successfully communicate with TLE4999C8 using SENT interface, however we are not able to verify the 8 bit CRC.
Could you please help us with some sample code to calculate the 8bit CRC for the short serial message format and SPC.
Thank you,
Jannick
Show LessHow to test the delay time in 5012B? More accurately, it is the delay time from testing the rotor position offset to MCU collecting this offset amount
Show Less