Dear Supporter
I want to translate the following KBA. Please confirm to my work.
What is the TLE5014 and what are some of its features?
Regards,
Nino
Show LessHi sir
I need a tilt sensor, is there a corresponding product recommendation?
Now I am designing the interface circuit for TLE5046iC-AK-LR. This device is compliant to Version: “Requirement Specifications for Standardized Interface for Wheel Speed Sensors with Additional Information “AK-Protocol” Version: 4.0 13.02.2008 of Daimler AG”
May I have this protocol doc? Or do you know where to get it?
Show LessDear Sir & Madam,
I am Gonul Demir from Fenac.
You can visit our website to get to more information about us. https://www.fenac.com.tr/
We have a new project. We are designing gear tooth sensor, but our target is not a standart gear.
The target is on the attachment file.
Radius is 90mm and there are 4 gear tooth on the target.
Our custermer need speed and direction information.
Output 1 should be digital square wave and measures the speed of target gear .
Output 2 is a DC level that when the target wheel rotates clockwise, the output signal 2 produces logic High, and when the target wheel rotates counter clockwise, the output signal 2 produces logic low.
Do you advice us your suitable speed sensor ?
Show Less
Hi,Partners.
What does Parameter-Not operational lifetime meaning? Is that storage temperature?What's the difference between normal operating and Not operational.Thanks.
Show Less