Adapters and Chargers Forum Discussions
Hi. Infineon
In my application; use 3172P to design in type-C adapter. now, the QC2.0 and QC3.0 OCP test data as below,230V AC input ,the QC2.0 and QC3.0 12V2.5A and 20V 1.5A OCP test result is 3.44A and 2.32A. I try to modify the battery.charging.h QC_AMP_20V(300 -->210 and 110) and QC_AMP_12V(300-->110 and 90) , but the test ressult without any change. would you like to let me know where to change to let the OCP meet customer requirement. and add schematic in here.
thanks
flance fang
12V2.5
Applications for CCG3PA in the datasheet only show connections to Type-C Receptacles.
Final systems, where this application are used, will convert the Type-C Receptacle to a Type-C Plug via a USB-C cable. The cable adds a pulldown resistor, Ra, of about 1k ohm and possibly a, EMCA device. If connecting a CCG3PA directly to a Type-C Plug, one CC line can be tied via 1k ohm to ground to provide symmetry. Are any other changes required from the basic design in Figure 8 of the CCG3PA datasheet?
Is the EMCA functionality needed if the physical cable isn't present?
What else is missing? Will CCG3PA software support the "Plug" configuration shown below?
Reference CCG3PA datasheet @ https://www.infineon.com/dgdl/Infineon-EZ-PD(TM)_CCG3PA_Datasheet_USB_Type-C_Port_Controller-DataSheet-v09_00-EN.pdf?fileId=8ac78c8c7d0d8da4017d0ee438366ac0
Show Less- « Previous
-
- 1
- 2
- Next »