Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
User22771
Level 1
Level 1
Hi,

is there any sample code for this? I'm not able to make it or reconfigure the size with WinIdea for TC36x
0 Likes
2 Replies
NeMa_4793301
Level 6
Level 6
10 likes received 10 solutions authored 5 solutions authored
DCON0 and PCON0 are ENDINIT protected, so you have to disable CPU ENDINIT protection to change them. Here's how the iLLD does it:

static void __Core0_start(void)
{
unsigned short cpuWdtPassword = Ifx_Ssw_getCpuWatchdogPasswordInline(&MODULE_SCU.WDTCPU[0]);

Ifx_Ssw_clearCpuEndinitInline(&MODULE_SCU.WDTCPU[0], cpuWdtPassword);

/* Enable/ Disable the caches depending on the configuration. At this point cache are invalidated */
{
Ifx_CPU_PCON0 pcon0;
pcon0.U = 0;
pcon0.B.PCBYP = IFX_CFG_SSW_ENABLE_TRICORE0_PCACHE ? 0 : 1; /* depending on the enable bypass bit is reset/set */
Ifx_Ssw_MTCR(CPU_PCON0, pcon0.U);
Ifx_Ssw_ISYNC();
}

{
Ifx_CPU_DCON0 dcon0;
dcon0.U = 0;
dcon0.B.DCBYP = IFX_CFG_SSW_ENABLE_TRICORE0_DCACHE ? 0 : 1; /* depending on the enable bypass bit is reset/set */
Ifx_Ssw_MTCR(CPU_DCON0, dcon0.U);
Ifx_Ssw_ISYNC();
}
User22771
Level 1
Level 1
Hi,

thanks a lot it works at least for configuring the PCon0/DCon0. But to visit the area reserved for DCache , eg for TC365 it should be 7003 C000H - 7003 FFFFH, i have also to set the CPU0_DCMAP?

Best Regards
0 Likes