Announcements

Robots are revolutionizing our lives in many ways. Join our webinar to learn about Infineon’s broad portfolio of robot building blocks.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

IvanoBono
Level 3
Level 3
10 sign-ins 10 replies posted 10 questions asked

hi all, using a illd, I configured a fast compare channel like this:

 

void FastCompare_Init(void) {
IfxEvadc_Adc_FastCompareChannelConfig config;
IfxEvadc_Adc_initFastCompareChannelConfig(&config,&g_evadc);
config.fastCompareChannelId=IfxEvadc_GroupId_14;
config.channelEventMode=IfxEvadc_ChannelEventMode_aboveOrBelowCompareValue;
config.serviceRequestGenerationEvent=IfxEvadc_FastCompareServiceRequestGeneration_newResult;
config.referenceValue=256;
config.runMode=IfxEvadc_FastCompareRunControl_alwaysRun;
config.triggerInterval=0; //16/fADC 16/160mhz= 1mhz
IfxEvadc_Adc_FastCompareChannel fc;
IfxEvadc_Adc_initFastCompareChannel(&fc,&config);
g_evadc.evadc->FC[fc_channel].FCHYST.B.DELTAMINUS=0; 
g_evadc.evadc->FC[fc_channel].FCHYST.B.DELTAPLUS=128; 
	volatile Ifx_SRC_SRCR* src_regP=IfxEvadc_getSrcAddress(IfxEvadc_GroupId_14,0);
	IfxSrc_init(src_regP, Cpu_GetCoreServiceProvider(), ISR_PRIORITY_FASTCOMPARE); 
	IfxSrc_enable(src_regP);
}

IFX_INTERRUPT(ISR_ADC_result, 0, ISR_PRIORITY_FASTCOMPARE);
void ISR_ADC_result(void)
{
	counter++;
 }

 

and it works as expected.

but,

it'is possible route interrupt to a TIM counter to perform Count or Frequency calc without cpu intervention?

I have already configured the TIM counters to detect a frequency or a count of a signal coming from a pin, but I don't understand how I can select the result of the fast appear as the TIM input.

0 Likes
5 Replies
Nambi
Moderator
Moderator
Moderator
250 replies posted First like given 25 likes received

Hi,

It is possible to route the FC BFL flag to TIM input.

You can refer to the section "Port to GTM TIM Connections" in the device-specific user manual for the device-specific routing options.

Best Regards.

0 Likes

i'am using TC377. I have already read this section and noticed that in the file:
"IfxGtm_PinMap.c" there is the mapping of all the configurations but there are not those of the FC BFL.
so i did this TIM init function :

 

IfxGtm_Tim_In g_driverTIM;	// TIM driver structure

void Tim_Init(void) { //test
    IfxGtm_enable(&MODULE_GTM);                                  //Enable the GTM
    IfxGtm_Cmu_enableClocks(&MODULE_GTM, IFXGTM_CMU_CLKEN_CLK0); //Enable the CMU clock 0
    IfxGtm_Tim_In_Config configTIM;
    IfxGtm_Tim_In_initConfig(&configTIM, &MODULE_GTM);   //Initialize default parameters
    //pin map for: FC2BFL, EVADC boundary flag level of FC channel 2
    static const IfxGtm_Tim_TinMap IfxGtm_TIM0_2_FC2BFL_IN = {IfxGtm_Tim_0, IfxGtm_Tim_Ch_2, {0}, (IfxGtm_ChXSel)0}; 
    configTIM.filter.inputPin = &IfxGtm_TIM0_2_FC2BFL_IN;           //Select input port pin
    configTIM.filter.inputPinMode = IfxPort_InputMode_undefined;    //Select input port pin mode
    IfxGtm_Tim_In_init(&g_driverTIM, &configTIM);           //Initialize the TIM
}

 

and in main i call:

FastCompare_Init();

Tim_Init();

and in main loop i read period with:

 

IfxGtm_Tim_In_update(&g_driverTIM);
int period=IfxGtm_Tim_In_getPeriodSecond(&g_driverTIM);

 

but it does not work. I forgot something?

0 Likes
Nambi
Moderator
Moderator
Moderator
250 replies posted First like given 25 likes received

Hi,

Can you check the "GTM_TIM_Capture_1" example from the Aurix Development Studio? 

1. You can test check this "GTM_TIM_Capture_1" existing TIM example at your end and ensure that it is successful.

2. Once you have a working example for TIM, you can adapt it for "fast compare ADC to TIM" mapping.

Best Regards.

0 Likes

i have a"GTM_TIM_Capture_1" example working, but how  adapt it for "fast compare ADC to TIM" mapping?

in init_TIM() function:

void init_TIM(void)
{
    IfxGtm_enable(&MODULE_GTM);                                         /* Enable the GTM                           */
    IfxGtm_Cmu_enableClocks(&MODULE_GTM, IFXGTM_CMU_CLKEN_CLK0);        /* Enable the CMU clock 0                   */

    IfxGtm_Tim_In_Config configTIM;

    IfxGtm_Tim_In_initConfig(&configTIM, &MODULE_GTM);                  /* Initialize default parameters            */
    configTIM.filter.inputPin = &PWM_IN;                                /* Select input port pin                    */
    configTIM.filter.inputPinMode = IfxPort_InputMode_pullDown;         /* Select input port pin mode               */
    IfxGtm_Tim_In_init(&g_driverTIM, &configTIM);                       /* Initialize the TIM                       */
}

 what should I set in
"config TIM.filter.inputPin config"

and

"TIM.filter.inputPinMode"
to select the "FC BFL flag"?

0 Likes
Nambi
Moderator
Moderator
Moderator
250 replies posted First like given 25 likes received

Hi,

In the example, this specific sequence calls IfxGtm_PinMap_setTimTin(), which is more relevant to using a pin as an input.

You can try to use IfxGtm_Tim_Ch_setTimTin() ILLD API for your requirement.

Best Regards.

0 Likes
This widget could not be displayed.