Hi Supporter
我的问题如题。前期开发阶段通过miniWiggle tool DAP 协议 debug TC377。目前正式产品需要提供ETK接口。
问题是ETK接口是16Pin的,miniWiggle的 DAP接口是10Pin的,接口不兼容。我想知道ETK接口中支持的DAP协议同miniWiggle中支持的DAP协议是否兼容。我是否可以通过做一个转接板的方式,将ETK接口中DAP协议相关的Pin脚转接到miniWiggle接口中DAP的对应Pin脚上。使得两个debug工具通过同一接口实现其相应的功能。还是说需要通过专用的转接工具来实现这一应用需求?
miniWiggle接口定义:
ETK接口定义:
已解决! 转到解答。
If the ETK interface contains the following pins for connecting to the DAP using the MINIWIGGLER. You can test the connection first by pulling out the wires before making the board.
Hi Jeremy!
因为要确定PCB的方案,因此我需要一个确定的答案。这样做是否可行,两个接口中的DAP协议是否完全兼容,如果不完全兼容的话,是在哪种条件下存在问题。
不知是否有对这块比较了解的大咖,给个解答。因为方案定了,板子发出去,如果有问题,影响会很大。
If the ETK interface contains the following pins for connecting to the DAP using the MINIWIGGLER. You can test the connection first by pulling out the wires before making the board.