- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
HI:
I need some help on how to setup Aurix Studio to work with custom board(our sample board based on TC277 Applicate Kit reference board).
I tried flash the board I got following error message :
Unhandled Exception: System.IO.FileNotFoundException: Could not load file or assembly 'System, Version=4.0.0.0, Culture=neutral, PublicKeyToken=b77a5c561934e089' or one of its dependencies. The system cannot find the file specified.
at AurixFlasher.Program.Main(String[] args)
Flashing failed
For Debugging, the following Error message came out:
Starting Debugger...
The debug instrument IO could not be initialized.
The GDI debug instrument provided the following error message.
An internal error has occurred.
Using Debug Target Configuration:
Target: Generic Infineon AURIX Board
Selected CPU type: tc27xd
Register file: C:/Infineon/AURIX-Studio-1.9.0/plugins/com.tasking.ctc.debug.win32.x86_64_1.12.14.0/ctc/include/sfr/regtc27xd.xml
Communication: Universal Debug Access Server
Debug Instrument Module: gdi2mcdtc
Using Flash Configuration:
Monitor : C:\Infineon\AURIX-Studio-1.9.0\plugins\com.tasking.ctc.debug.win32.x86_64_1.12.14.0\ctc\etc\ftc27x.sre
Workspace address : 0x70000000
Number of devices : 5
Sector buffer size : 8192
Device 0:
Address : 0xA0000000,0x80000000
Vendor : Infineon
Chip : TC2_4560k
Subname : Program Flash 0
Width : 32
Size : 2097152
Number of chips : 1
Unused address lines : 0
Device 1:
Address : 0xA0200000,0x80200000
Vendor : Infineon
Chip : TC2_4560k
Subname : Program Flash 1
Width : 32
Size : 2097152
Number of chips : 1
Unused address lines : 0
Device 2:
Address : 0xAF000000
Vendor : Infineon
Chip : TC2_4560k
Subname : Data Flash Bank 0a
Width : 32
Size : 393216
Number of chips : 1
Unused address lines : 0
Device 3:
Address : 0xAF100000
Vendor : Infineon
Chip : TC2_4560k
Subname : Data Flash Bank 0b
Width : 32
Size : 16384
Number of chips : 1
Unused address lines : 0
Device 4:
Address : 0xAF110000
Vendor : Infineon
Chip : TC2_4560k
Subname : Data Flash Bank 1
Width : 32
Size : 65536
Number of chips : 1
Unused address lines : 0
Configuration: TC27xD
Starting Debugger...
The debug instrument IO could not be initialized.
The GDI debug instrument provided the following error message.
An internal error has occurred.
How to configure or setup Aurix Studio project to get around this problem?
Thank you
James
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi James, do you have triboard or other board? And have you downloaded proper software for the board?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi:
This is few update on some finding. We are in the process of bringing up our own custom board design(based on the reference design). The development tool of our choice is using Aurix Studio + DAP miniWiggler. According to our hardware engineer, the TC277 is production version on our custom board. Once flashed Aurix Stuido generated debug image via DAP, the MCU got into no recoverable state after debug reset. I used DAS tool for MUC detection. A message " Device is locked" is appeared.
The following are the questions:
- Why and how MUC(TC277) would get into this "locked" state?
- Could we debug TC277 production chip using Aurix Studio and DAP? And how to set it up?
- If MCU(TC277) got into this "locked" state, how to get MUC out of this state?
Thank you fort the help!!!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Please flash the default software into the chip, if you use your own software, you should check if any password is written to UCB. If you has password, sometimes you can unlock but it depends. You can review the Triboard user manual and software here.(Note: myICP required)
We can debug the triboard with miniwiggler and ADS, but you first should use a triboard and default software. I don't know what is your source code and your board.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi:
Thanks for the suggestion. However, we have encountered a issue of not able to flash the image even using Lauterbach debug. To get some understanding, what is this default software? Is this default software from Aurix Studio project creating process?
Thank you
James
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
If you have a Triboard and installed ADS, you can import from File menu, or access github for the default software, for example the code is used to blink the LEDs.