Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
zpedro
Level 1
Level 1
First reply posted First like given First question asked

Hi,
In order to prepare a MOL (Middle Off Line) test system, we need to add an industrial programmer to in case of UUT firmware  is not actualised, update it during the process in this station.
I need the "flash programming specification" of the device these information/documentation need to be detailed for we implement the flash/programming algorithm.
Many Thanks!
José,

0 Likes
1 Solution
Meet_T
Moderator
Moderator
Moderator
100 solutions authored 25 likes received 50 solutions authored

Hi @zpedro ,

 

For this the section 6.5 Data Memory Unit (DMU) from the user manual can be referred, DMU facilitates all operations executed on the PFLASH and DFLASH memories. You can also find the command sequences for the flash mentioned in section 6.5.2.2.2 Command Sequences.

 

If you want any reference program regarding how to flash the PFlash you can refer to the following code example Flash_Programming_1_KIT_TC375_LK, you can find the presentation associated with this code example here Flash_Programming_1_KIT_TC375_LK.

 

This example is for TC375, this is also available for TC334 and TC397 in the Aurix Code Example github repository. You can choose one based on the device you are using and adapt it (change pins and other configurations) if required. 

 

BR,

Meet,

View solution in original post

2 Replies
Meet_T
Moderator
Moderator
Moderator
100 solutions authored 25 likes received 50 solutions authored

Hi @zpedro ,

 

For this the section 6.5 Data Memory Unit (DMU) from the user manual can be referred, DMU facilitates all operations executed on the PFLASH and DFLASH memories. You can also find the command sequences for the flash mentioned in section 6.5.2.2.2 Command Sequences.

 

If you want any reference program regarding how to flash the PFlash you can refer to the following code example Flash_Programming_1_KIT_TC375_LK, you can find the presentation associated with this code example here Flash_Programming_1_KIT_TC375_LK.

 

This example is for TC375, this is also available for TC334 and TC397 in the Aurix Code Example github repository. You can choose one based on the device you are using and adapt it (change pins and other configurations) if required. 

 

BR,

Meet,

zpedro
Level 1
Level 1
First reply posted First like given First question asked

Thanks Meet!

0 Likes