Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Struppi
Level 1
Level 1
First reply posted First question asked First like given

Dear Readers,
I am part of a team which migrates a single core software to a multicore.
The software is now running on one core properly.
In the very first step we want to duplicate the software on a second core.
Therefore we want to clone all functions with exception of the hw intimate ones.

How can that be done, that function void Foo( void ) runs twice on two cores?
We use the Hightec toolchain.

Any hints are appreciated!

Regards
Struppi

0 Likes
1 Solution
µC_Wrangler
Employee
Employee
50 solutions authored 100 sign-ins 25 likes received

Hi Struppi.  In that case, it's very possible to build separate applications (separate elf/hex files).  It's just a matter of having CPU0 start CPU1 from the right address.  For example, assuming you're using a TC39x:

CPU0 would use its own linker file, using PFLASH from 0xA0000000-0xA02FFFFF, and RAM from 0x70000000-0x7003BFFF

CPU1 would use a separate linker file, using PFLASH from 0xA0300000-0xA05FFFFF, and RAM from 0x60000000-0x6003BFFF

At startup, CPU0 would need to set CPU1s PC to 0xA0300000, then start it.

The PFLASH addresses are very negotiable - you could have both CPUs execute from the same bank if necessary.  Having them build into separate PFLASH banks will get you the best performance.

View solution in original post

4 Replies
µC_Wrangler
Employee
Employee
50 solutions authored 100 sign-ins 25 likes received

Hi Struppi.  There is typically no need to duplicate the function, because the default configuration allows every CPU core to access all of PFLASH.  If Foo() is using global variables, then you do have to be careful about managing concurrency, through semaphores, etc.

In applications where performance is absolutely critical, you might want to copy Foo() into PSPR (Program Scratchpad RAM), and execute from that.

0 Likes

Hi µC_Wrangler,

>is using global variables

we have tons of that and we want to avoid - at the beginning at least - to tackle with concurrency.
Is there no way? ( Flashing cores individually?,... )
Regards
Struppi

0 Likes
µC_Wrangler
Employee
Employee
50 solutions authored 100 sign-ins 25 likes received

Hi Struppi.  In that case, it's very possible to build separate applications (separate elf/hex files).  It's just a matter of having CPU0 start CPU1 from the right address.  For example, assuming you're using a TC39x:

CPU0 would use its own linker file, using PFLASH from 0xA0000000-0xA02FFFFF, and RAM from 0x70000000-0x7003BFFF

CPU1 would use a separate linker file, using PFLASH from 0xA0300000-0xA05FFFFF, and RAM from 0x60000000-0x6003BFFF

At startup, CPU0 would need to set CPU1s PC to 0xA0300000, then start it.

The PFLASH addresses are very negotiable - you could have both CPUs execute from the same bank if necessary.  Having them build into separate PFLASH banks will get you the best performance.

Thank you!

0 Likes