AURIX™ Forum Discussions
您好!我想请问一下关于OTA的文件应该去哪里获取?P32404-Tutorial_Using_the_2nd_Generation_AURIX_SWAP_mechanism_for_SW_updates_Over_The_Air_v1.1
Hello All,
I am working on the EVADC Configurations for TC377, I am having the Hardware triggers on the channels of
G0ch6 - ATOM1_5 (not working)
G0ch7 - sync with G2ch7
G1ch1 - ATOM1_4
G1ch2 - ATOM1_4
G1ch6 - ATOM1_5
G1ch7 - sync with G2ch7
G2ch6 - ATOM1_4
G2ch7 _ ATOM0_7
G3ch6 - ATOM1_7 nd ATOM2_4
G3Ch7 - ATOM1_7 nd ATOM2_4
G8ch0 - Sync with G10ch0
G8ch3 - ATOM1_4 (not working)
G9ch0 - Sync with G10ch0
G10ch0 - ATOM1_7
G11ch0 - Sync with G10ch0
In this ,Group 0 and Group 8 channel Hardware triggers are not working. As it is the first group from primary and secondary, I have to do any extra configurations for those channels? or any other suggestions to run the Hardware trigger.
Kind regards,
Sailesh.
Show Less
I tried to read a register value of I2C device(pressure sensor based on the I2C bus transmission signals(refer to attachment) described by the sensor datasheet.
Could anyone show me how to generate the repeated start signal or provide the sample code. Thanks
//iLLD Libraries used by program
uint8 i2cTxBuffer[1] = {WHO_AM_I_REG};//WHO_AM_I_REG: register address
uint8 i2cRxBuffer[1]
/* Write data to device */
while(IfxI2c_I2c_write(&g_i2cDevPressure, &i2cTxBuffer[0], 1) == IfxI2c_I2c_Status_nak)
/* Read the data*/
while(IfxI2c_I2c_read(&g_i2cDevPressure, &i2cRxBuffer[0], 1) == IfxI2c_I2c_Status_nak)
Show Less
Hi All,
I'm trying to read out the current counter value of STM0.TIM0, my question is that do I need to disable all interrupt before I read counter. From my opinion, the processing of reading counter may be affected by other interrupts, which may cause I read a wrong value from register. For example, one interrupt is triggered when I just only read out the lower 16-bit of counter value, so that the higher 16-bit value can only be read out after process the interrupt function. Then I get a wrong value.
Can anybody help me explain this?
thanks so much.
Show Less
Background:
1. FreeRTOS was ported into KIT_A2G_TC397_5V_TFT;
2. FreeRTOS-Plus-TCP was ported without NetworkInterface.
3. Built and downloaded, the functions worked well but TCP.
Anybody has the example for RTL8211FI-CG, expect your help.
The source code link:https://github.com/Lucas20220329/PLS_RTOS.git
Show LessHi, there!
I first download an elf to a new tc234 board by lauterbach, and it is successful. When reset the board, I can't download the same elf to the same board again.
I use the DAS basic client to connect the board, it shows "DAS Error:Device_locked".
This is the BMHD I configured:
const uint32 BootModeHeader_0[] = {
0xA0000020u, /* STADBM first user code at 0x8000 0020h */
0xb3590070u, /* BMI = 0070h BMHDID = B359h */
0x00000000u, /* ChkStart */
0x00000000u, /* ChkEnd */
0x00000000u, /* CRCrange */
0x00000000u, /* !CRCrange */
0x5DB996ACu, /* CRChead */
0xA2466953u /* !CRChead */
};
Anyone know why the borad is locked?
Show Less
Hello everyone,
After successfully enabling SWAP mode on TC375, the link files of the two programs were first changed and divided into AB partitions corresponding to the two programs. The function of program A is to make alternative mapping active, while the function of program B is to flash the LED light.
When the standard is active, both programs are simultaneously downloaded into the controller through the Infineon downloader. After powering on, A runs normally, powers down, and then powers up again, successfully making the alternative active. However, the LED not flashing, and the B program fails to run. May I ask how to solve it?
The following is the modified link file
Show Less