AURIX™ Forum Discussions
text.format{('custom.tabs.no.results')}
HI, experts:
I want to get the full version of the demo software for motor control of TC334L chip, where can I get it? If Infineon has it, please send it to me, thank you!
In Familiar, Infineon's " Infineon Developer Center Launcher " Tool Does Not Provide Any Motor Control Software for the T3X series, but Infineon's official documentation states that the software is available:
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/AURIX/How-to-get-TC334L-chip-about-motor-control-full-version-demo/td-p/645023
Show LessHi community,
I'm trying to implement SPC communication with a TC27xD. I am able to send the SPC trigger and receive the response using 2 different pins : 1 for input and 1 for output.
However, when using a single pin, I feel like the port stays in output mode and never switches to input mode. I can see the trigger being sent but am struggling to receive the response frame.
I have set the SENT channels as :
Hello,
Can the FLSLoader be used to program the UCB_BMHD ?
Thank you,
Aditya
These bits are getting set after enabling the FSP reaction for this , observation is sometimes this is happened while connecting the debugger (trace32) only. and if we disable the reaction then this is not observed sometimes . Is there any specific reason for this like CPU load ,
please help me out in this .
Show LessTC397 UCB区间段被擦除后,DAP miniwigger 连接不上是什么原因,怎么解决,求老师指教
I used hightec toolchain in aurix developpment studio and comiled demo ILLD_TC397_ADS_FreeRTOS_Basic, what should i do to compile it in GCC?
Show LessHi Infineon Expert:
I'm using TC3XX series, I want to use the TIM_EXT_CAP feature as the INPUTSRC to measure an outside PWM signal's period and dutycycle, Is it possible to use the connection in below picture?
BR,
Zhang
Show Less
报错使用的工程是基于ASCLIN_UART_1_KIT_TC397_TF这个demo,添加了一些autosar工程和生成代码。
使用的ADS版本是1.5.2,编译完成后没有报错,随后进入到Debug时,弹出以下提示:
随后我又下载了demo进行实验,发现demo能够正常进行调试:
这个debug问题该如何解决呢?
#TC397
Show Less