AURIX™ Forum Discussions
自媒体一直在网上高歌中国的新能源汽车遥遥领先,连奔驰,宝马,大众,奥迪,丰田本田在新能源汽车上不敢跟中国叫板,已经在技术上落后中国车企,那么在汽车物联网以及电控控制的芯片都是用哪些品牌的?
问题链接:https://www.zhihu.com/question/615157930
可以谈谈新能源汽车市场情况和发展趋势,以英飞凌产品为案例,对汽车物联网和电控控制的芯片进行介绍。
Show LessHi all,
our company have signed NDA with infineon, and We have MyICP access. But we can not find document "HSM Target Specification – Rev 2.0 " and related demos in AP32349? How can we get these related documents and demos?
looking forward for your help.
Show Less
Dear Team,
We are interested in the part SAK-TC324LP-16F1 60F for motor inverter and control design in automotive. In Infineon portal, part status was mentioned as "on request". Would you please confirm the part status and end of life for the part?
Show LessHello, I was checking interrupt handling but I couldn't understand well. Can you please answer below questions?
User manual says there are 1024 interrupt trigger vector and you can see above there are 1024 Service Request Control Register (SRC), I couldn't find which one is which in reference manual. Is there any table like below which says which number has which interrupt source?
I was examining ASCLIN_Shell_UART_1_KIT_TC375_SB (Aurix Development Studio example) and saw this:
We are giving function address to put vector table with "isr", core that will execute function with "vectabNum", priority with "priority". How hadrware knows which function to execute when new data is received? Because we didn't give any index to that macro so how it knows which index of vector table to put? Thanks.
Ali
Show LessHello,
I am coding on AURIX_TC377, I got the following linking error which I am not sure how to solve.
ltc E112: cannot locate 4 section(s):
ltc I455: requirement: 1M (0x15eb80) bytes of RAM area in space mpe:vtc:linear
ltc I456: section type: range restriction - range(s) 0x70000000-0x70032800
ltc I456: section type: group restriction - contiguous
ltc I457: bss_SEC (84546) (0x15cc20 bytes)
ltc I457: data_SEC (84547) (0x1f5c bytes)
ltc I457: zbss_SEC (84548) (0x2 bytes)
ltc I457: zdata_SEC (84549) (0x2 bytes)
seems that after integrating a new plugin, the size allocated is not enough anymore. But I am not sure what I should change to make it suitable again.
For example. blocksizefor bss_SEC in .lsl =2, the ltc I457: bss_SEC (84546) (0x15cc20 bytes)
My unfamiliarity with linkerscript making it hard for me to figure out the issue regarding these 4 sections. Appreciating your help in advance
I attach .lsl and for your reference.
PS. I tried to check the .map searching with any allocated sections with all zeros 0x00000000 but found nothing.
I have attached a zip file which consists of the linker file (.lsl) and .map files
Show Less
Hello,
in the Infineon-SAK-TC37x-DataSheet-v01_01-EN.pdf Page 188 on e.g. AN4 EVADC_G11CH0 as well as EVADC_G0CH4 is listed.
Is it possible to sample AN4 during runtime in parallel in G11 and G0?
My Idea would be following: While having AN4 in G0 sampled with Channelneigbours e.g. AN2 and AN3 in "continuous mode" as fast as possible and with activated Limit Checking (=> continuous Over/UnderValueProtection), in parallel to that AN4 shall be sampled in G11 depending on GxREQGTA GTM_adcx_trig0 (also cyclic during runtime). Depending on the timing here and there will be a simultaneous sampeling in G0 und G11.
This is in general possible, right? Is there anything special to be considered?