Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

AURIX™ Forum Discussions

zhlei327
AURIX™
After I install DAS_V7_3_7_SETUP.exe and restart my laptop,  Infineon-Memtool-DevelopmentTools-v06_00-EN.exe can connect the TC387. I want to use DAS... Show More
AhmedSayed
AURIX™
Hello all,I'm currently trying to migrate into a Linux system, but noticed that the Bifaces framework I had was for Win64 systems.I was wondering if t... Show More
Jonson
AURIX™
HI,expert: 在TC334的例程中看到这样的代码:   我感到奇怪的是: 1.这里的“.samplePoint = 8000,”是什么意思,为何设置8000,意味着采样点是80%? 2.一般同步段长度不都是1Tq吗?这里怎么设置“.syncJumpWidth = 3”,是基于什么考虑? 3... Show More
michaelxing
AURIX™
多核处理
solved msg Solved

你好,我想咨询英飞凌TC系列MCU多核如何处理同步和互斥,自锁锁怎么使用?

Translation_Bot
AURIX™
A new project, planning to do EVCC. Is there any relevant open source code or board --- The ISO 15118 specification defines an IP-based data communic... Show More
Harish_21
AURIX™
Hi , I was trying to inject error for testing Alm8[22]. i had gone through the SCRi register and also referred 16.4.1.9 section for Error injection. I... Show More
Translation_Bot
AURIX™
Hello, Infineon: ATOM can also directly write to registers without an ARU, thereby configuring the duty cycle and cycle. My question is what is happen... Show More
Translation_Bot
AURIX™
Regarding the ADS Tasking linker file, change the defined variable from the original PFLASH to the DFLASH location. Assuming I define a variable in th... Show More
Kumaresh
AURIX™
Hi, Is there any example on how to use external generate carrier wave instead of aurix generated excitation wave in DSADC? Background: I am trying to ... Show More
jqk
AURIX™
"IfxGtm_Tom_Timer_Config" “triggerOut” seems to be used to trigger the ADC, does it have something to do with the “timerChannel”?  “triggerPoint”seems... Show More
Forum Information

AURIX™

In this forum you can post your questions, comments and feedback about the 32-bit AURIX™ TriCore™ Microcontroller. The AURIX™ offers the highest scalability in performance, memory & peripherals across application. It is a safe and secure companion chip, meeting both the ISO functional safety standards and EVITA full security standards. Here you can also find the links to the latest board pages, SW and Tools GitHub, trainings, documents and FAQs