Announcements

Help us improve the Power & Sensing Selection Guide. Share feedback

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

AURIX™ Forum Discussions

User14049
AURIX™
Hi,


I am working on Autosar, can anyone help me to know which tools to be use to generated code for different layers of Autosar.
lord_feistel
AURIX™
Hello, I bought an evaluation board KIT_A2G_TC397_5V_TFT . I doing some experiments and some question rose up I saw there is the BROM ( Boot Rom ) whi... Show More
dev85
AURIX™
Query is related to Infineon Aurix TC3xx & TC2xx controllers: To utilize HSM hardware capabilities (for storing keys, utilizing crypto engine) in TC2x... Show More
long
AURIX™
hello, I have some questions about the interrupt . when a interrupt is running ,can another higher priority interrupt run ? can a trap event interrupt... Show More
bhagapll
AURIX™
I am trying to analyze the possibility to use the GTM for engine position detection and Fuel injector actuation with TC38x to minimize the CPU load. I... Show More
bhagapll
AURIX™
I am trying to analyze the possibility to use the GTM for engine position detection with TC38x to minimize the CPU load. Where I can find the example ... Show More
do-while
AURIX™
sent接收
solved msg Solved
我在sent接收的过程中遇到了下面问题 接收的第一帧数据正常,后面接收的数据FIR中断标志位就会置1(This bit is set after a Synchronization / Calibration pulse was received that deviates more than +-... Show More
koala
AURIX™
In my application, HSPDM triggers EVADC to sample two channels simultaneously. How should I configure EVADC to minimize sampling jitter and also maxim... Show More
TippleM
AURIX™
Hi, I use miniwiggler debugger for debugging TC3972 MCU, but it is really slow. I have just code debugging application and safety or DSP debugging sup... Show More
Nikhil_U
AURIX™
Hello, I am using the TC377_SEC _GTW controller, as I need to remove the loopback of the CAN, and have to make transmit\receive for external PCAN. So,... Show More
Forum Information

AURIX™

In this forum you can post your questions, comments and feedback about the 32-bit AURIX™ TriCore™ Microcontroller. The AURIX™ offers the highest scalability in performance, memory & peripherals across application. It is a safe and secure companion chip, meeting both the ISO functional safety standards and EVITA full security standards. Here you can also find the links to the latest board pages, SW and Tools GitHub, trainings, documents and FAQs