AURIX™ Forum Discussions
Hello Infineon,
I am facing issue with SPI communication . Getting SPI sequence as pending. and as GLOBALCON1.ERRORENS = 7F .
what are supposed reasons for pending Sequence ? How can i debugg the issue. Please reach me out as soon as possible , its urgent.
regards,
Ashwini
Show Less
在进行ADC采集的时候,发现有一路的结果寄存器GxRESy里面的有效标志位valid flag(VF)一直为0,导致程序一直卡在一直验证VF是否有效这个地方(do while(!VF)),请问各位有遇到过这个问题吗?应该怎么解决啊
使用ADS软件编译程序卡住在40%,此时显示编译已经基本结束,CPU(因特尔i9-13)占用率从80%降低到5%,说明此时CPU基本已经停止编译工作。但是编译无法正常结束,卡住一小时后不得不停止编译。且查看不了正确的报错信息。编译ADS自带的TC297工作例程,也出现了类似的问题,只不过卡在16%,并且显示芯片的cpu0~cpu2都编译完成,但是还是卡住了...
Show Less如何在TC264或者TC377中使用FOC呢,GTM模块相关配置实在太过于复杂了,实在有一些看不懂,有没有什么相关的中文资料或者开源代码可供参考。
HI,expert:
目前我正在进行关于TC334芯片的BootLoader的开发,需要得到英飞凌工程师的相关支持,具体如下:
1.请帮忙评估一下我目前使用官方的板子“KIT_A2G_TC334_LITE”是否适合用于研究BootLoader开发,当然我有购买英飞凌官方的DAP烧录器;
2.能否提供给我关于TC334开发BootLoader的相关资料和源码例程;
以上需要英飞凌工程师的支持,谢谢!
Show Less
I am working with TC387 controller and observing around 100% CPU load when traffic on CAN bus is increased.
How CAN Traffic is increased-
By sending messages from Canoe at 1ms periodicity irrespective of their configured periodicity as per DBC file.
CAN is configured as Interrupt Based.
Impact of Increased CPU Load-
CAN communication stopped working due to increased load on Core0.
Communication stack is implemented on Core0.
Core Impacted-
CPU load is reaching peak on Core0 where the CAN messages from COM are received and processed and further shared to other applications.
Other cores are not impacted significantly due to increased CAN traffic.
Query-
What measures can be taken /checked in order to optimize the CPU Load due to CAN traffic increase so that CAN communication remain unaffected?
Show Less
Dear Madam, Sir,
We have programmed the BMHD0_ORGI to 0x8000_0000 flashed the internal application code thru TRACE32
we are getting continuous RESET along with crashing application after Power OFF and POWER
could you please let us know how to find the reason for this reset ?
Chip is not bricked, and we are able to flash application again and again .
thanks
Mohan
Show LessHello, Infineon:
May I ask how to operate the register under MCS (using C). I tried it on assembly before, and it worked, but I have no clue under C.
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/AURIX/GTM-MCS-%E4%BE%8B%E7%A8%8B/td-p/663666
Show Less