AURIX™ Forum Discussions
text.format{('custom.tabs.no.results')}
How to resolve the error with code 18003 in EB tresos?
Hi, I am working on linker files. I have a group like this:
group xyz (ordered, run_addr = mem:mpe:pspr0, copy)
{
select ".text.xyz";
} Iam trying to place the code in this PSPR section, but I am getting a linker error like: ltc E121: relocation error in "task1": relocation value 0x80225c20, type rel24 or abs24, offset 0x10, section ".text.CPU1_CODE" at address 0x7010028c is not a valid address in R_TRICORE_24REL. Hint: check the mapfile for a section that occupies this address.
ltc F019: unrecoverable error: fatal locate error. Can someone help me in resolving this?
Show LessHi, I have encountered ctc S9111:internal consistency check failed - please report an error using aurix development studio, how can I solve it?
Building file: ../src/sja1105.c Invoking: TASKING C/C++ Compiler ctc S911: internal consistency check failed - please report cctc -cs --dep-file="src/sja1105.d" --misrac-version=2004 -D__CPU__=tc39xb "-fD:/tc397/code-1222/tc397_fx/TriCore Debug (TASKING)/TASKING_C_C___Compiler-Include_paths__-I_.opt" --iso=99 --c++14 --language=+volatile --exceptions --anachronisms --fp-model=3 -O0 --tradeoff=4 --compact-max-size=200 -g -Wc-w544 -Wc-w557 -Ctc39xb -Y0 -N0 -Z0 -o "src/sja1105.src" "../src/sja1105.c" && \ make: *** [src/subdir.mk:43: src/sja1105.src] Error 1 if [ -f "src/sja1105.d" ]; then sed.exe -r -e 's/\b(.+\.o)\b/src\/\1/g' -e 's/\\/\//g' -e 's/\/\//\//g' -e 's/"//g' -e 's/([a-zA-Z]:\/)/\L\1/g' -e 's/\d32:/@TARGET_DELIMITER@/g; s/\\\d32/@ESCAPED_SPACE@/g; s/\d32/\\\d32/g; s/@ESCAPED_SPACE@/\\\d32/g; s/@TARGET_DELIMITER@/\d32:/g' "src/sja1105.d" > "src/sja1105.d_sed" && cp "src/sja1105.d_sed" "src/sja1105.d" && rm -f "src/sja1105.d_sed" 2>/dev/null; else echo 'No dependency file to process';fi make: *** Waiting for unfinished jobs.... TASKING VX-toolset for AURIX Development Studio (non-commercial): control program v1.1r8 Build 22011964 Building file: ../Cpu0_Main.c
Thanks.
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/AURIX/aurix-development-studio-%E6%8A%A5%E9%94%99ctc-S911-internal-consistency-check-failed-please/td-p/666241
Show LessHello:
The board is TC389, an explanation of the function FLSLoader_erase:
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/AURIX/%E4%BD%BF%E7%94%A8FlsLoader-Erase%E6%93%A6%E9%99%A4UCB%E7%9A%84%E8%AF%A2%E9%97%AE/td-p/671958
Show LessHi,
I am trying to modify KIT_AURIX_TC397_TFT , I want to start echoInit() function after I see all these steps on terminal. I am kind of stuck which functions are responsible to obtain this IP address. I reach near tcp_listen() function even before new ip is assigned. Can someone explain how I can change it?
Thank you,
Shivani
Show Less
Hello Infineon team!
I'm using ADS and working with ILLD and the 367DP MCU.
Literally, the assignment operator is not functioning as expected.
For example, consider the following code (this is an extremely simplified example, in reality, it involves assigning SPI results to a variable for output via CAN communication):
int a = 3;
int b = 0;
b = a;
When executing this code, b should be 3. However, b remains 0.
Has anyone experienced a similar issue? What solutions or checks should be considered in this case?
I am using ILLD and ADS (AURIX Development Studio) exclusively.
I'm using debugger(mini wiggler) and when i run code under debugging status with ADS, assignment is done very well,
but without debugger, when i run program, assignment is not working.
(i didn't mean whole assignment is not working. only some code lines are not working)
I'm not sure it is H/W problem(cache.. or something) or compiler(tasking) 's problem.
thank you.
Show LessSetup:
Infineon Memtool 4.9 on TriBoard with TC39x (BSL/ASC)
COM port to device set as Infineon DAS JDS COM port
Windows 11 - 23H2 Build 22631.2861
Device have been programmed before.
After Windows USB driver update the connection stopped working.
Error:
Controller0.Core0 - Can't establish Connection to Target
Error messages:
MiniMonTargIntf: Can't connect target !
MiniMonTargIntf: Failed to open serial port !
MiniMonTargIntf: Port error: Access is denied.
Error log and screenshots attached.
Show Less
Infineon Memtool 4.9 on TriBoard with TC39x (BSL/ASC)
COM port set as Infineon DAS JDS COM port
Windows 11 - 23H2 Build 22631.2861
Controller0.Core0 - Can't establish Connection
Show Lessi wanted to initialize TC277TF EMEM RAM(base address : 0xBF00000), memory trap was reported, and the values in those address were 0 , when i read it through IC5700:
Hello Together.
I wrote the following code to read the CCT_Timer Capture Registers and then calculate the Duty Cycle.
When I compile this Code with ADS, I get the following Error
main.c:(.text.code.main+0x8a): error: undefined reference to `__mulint_PARM_2'
main.c:(.text.code.main+0x95): error: undefined reference to `__mulint'
main.c:(.text.code.main+0xc5): error: undefined reference to `__divulong_PARM_2'
main.c:(.text.code.main+0xda): error: undefined reference to `__divulong'
Does anyone have an Idea where this Error comes from and how can I fix it?
thanks a lot in advance!! v
void main()
{
volatile unsigned int Capture_Value_1 = 0;
volatile unsigned int Capture_Value_2 = 0;
volatile unsigned long Capture_Value_sum = 0;
volatile unsigned long temp;
volatile unsigned char Duty_Cycle = 0;
while(1)
{
Capture_Value_sum = Capture_Value_2 + Capture_Value_1;
temp = (unsigned long )((unsigned int)Capture_Value_1 * 100);
Duty_Cycle = (unsigned char) ((unsigned long)temp /Capture_Value_sum);
}
Show Less