Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

AURIX™ Forum Discussions

baqian
AURIX™

你好,请问TC397最多支持3x4=12路CAN FD同时工作嘛?谢谢

Kevingiordano14
AURIX™
Hi community. I would like to ask you if it is possible to trigger a single EVADC channel through 2 trigger events of TOM. In detail, i would like to ... Show More
kunalsh
AURIX™
Unable to flash or program the SAL-TC275TP-64F200N DC custom board using AURIX Development Studio (ADS), despite successful connection with the core u... Show More
che
AURIX™
你好 目前使用"UART_VCOM_1_KIT_TC397_TFT"範例在Triboard TC397上進行測試。 開啟兩組ASCLIN 模組0跟模組4並且在中斷設置中有更改相對應的向量表數值,進行以下交互測試: 1. CPU0_Main.c內執行兩組ASCLIN初始化、只有調整"中斷向量表數值(0... Show More
shivani
AURIX™
Hi, I want to use analyzer tool from WinIdea debugger to do code profiling and I am launching the debugger from aurix development studio. I am facing ... Show More
MichailSkitsas
AURIX™
Hello community, I am very new to the ADS and one of the first things I noticed is that - by default - there is no autocomplete or automatic code tem... Show More
Translation_Bot
AURIX™
I have installed Infineon's free compiler Aurix Development Studio, which comes with iLLD, but the first time I compile it I always get an error, as f... Show More
Translation_Bot
AURIX™
The TC397 fails to brick for burn-in, consider entering BSL mode to re-burn it via the serial port. The related documentation mentions the need to "Up... Show More
irieyang
AURIX™
你好,在做MPU时,按照手册所述步骤对syscon寄存器的PROTEN位域写1后会进class1tin4(MPX)trap,随后是class3tin1最后进入class3tin4trap,以下是相关代码。对syscon写操作时PSW.IO为supervisor mode。 想问出现这种情况的原因以... Show More
Leej
AURIX™
We are looking for external RAM (around 2MB, possibly 8MB in the future, automotive qualified, -40deg to 125deg) to TC387 MCU in our project. However ... Show More
Forum Information

AURIX™

In this forum you can post your questions, comments and feedback about the 32-bit AURIX™ TriCore™ Microcontroller. The AURIX™ offers the highest scalability in performance, memory & peripherals across application. It is a safe and secure companion chip, meeting both the ISO functional safety standards and EVITA full security standards. Here you can also find the links to the latest board pages, SW and Tools GitHub, trainings, documents and FAQs