AURIX™ Forum Discussions
As in the title, if DMA accesses RAM, what types of RAM can it access, and can it access the LMU of each core
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/AURIX/Aurix%E7%B3%BB%E5%88%97%E5%8D%95%E7%89%87%E6%9C%BA%E7%9A%84DMA%E6%98%AF%E5%90%A6%E8%83%BD%E8%AE%BF%E9%97%AE%E5%90%84Core%E7%9A%84LMU/td-p/675567
Show LessTC39x芯片的BMHD中配置的Checker Software的作用是什么,在Checker 软件中都执行了哪些操作,这么设计的初衷是什么?
Hello, I want to supply microcontroller in single supply mode (Vext=5V) and I want the microcontroller to generate internally VDD (1.25V) and VDDP3 (3.3V).
I'm not able to find on your documentation which external components (MOSFET,inductor) I need to connect to EVC regulator. I just find these information for TC37x or higher.
Also, I'm not able to find VGATE1P and VGATE1N on microcontroller pinout. I've found VCAP pins but I don't know if they're part of EVC regulator.
Additionally, I don't know what is VDDO? This is a power supply different to VDD? What I need to connect to this?
Thanks for your help.
Regards,
AD
Show LessHi, please tell me how to adjust the size of the MCU SPI T51 and T510, as shown in the attached picture.
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/AURIX/TC397-%E5%A6%82%E4%BD%95%E8%B0%83%E8%8A%82SPI%E7%9A%84-timing/td-p/675568
Show LessI disabled ALM8[10] and ALM8 [17] in MCAL as shown in the picture, but these two errors are still reported in SMU AG8 on cold start, while WDG are working normally. However, if I reset the program with debugger, these alarms will not be reported. Can I have some suggestions? Thanks.
Show Less
As suggested by following table in user manual, For the TC357TA eval board I use, the maximum sampling rate should be 2.6 MHz:
But I cannot achieve this rate.
The first problem I encounter is that, using iLLD API, DIVA cannot be configured to 2, because in "IfxEvadc_initializeFAdcI" function, the maximum analog frequency is limited by IFXEVADC_ANALOG_FREQUENCY_MAX which is 20 MHz. Can I safely change IFXEVADC_ANALOG_FREQUENCY_MAX to 53333333, so that analog frequency can achieve 53.3 MHz as indicated in previous table?
Show Less
Hello Infineon,
I am confused about how PWM triggers EVADC conversion . How exactly this PWM triggers are generated. What should we take in considerations ?
Thanks and regards,
Ashwini
Show LessHello,
For the Tasking compiler integrated in ADS, we know that it requires purchase of a license for production. Can it be used at only development stage in a commercial project?
Show LessHello,
We are new to AURIX platform. We are looking for a safety RTOS. In the past we used Azure RTOS in our applications with other microcontrollers. For AURIX platform, is there any port for it? It now becomes the only open source safety certified RTOS in the market. Does Infineon plan to support it? It can be very attractive for all customers.
Show Less