AURIX™ Forum Discussions
Hi,
In a every Can node there are 16 groups of interrupt which can be routed to INT_lines IfxCan_InterruptLine_0..15.Is it possible to enable 2 or more IR **bleep**s, an to attach different Interrupt Service Routines. For example :
NodeConfig.interruptConfig.transmissionCompletedEnabled = TRUE; NodeConfig.interruptConfig.traco.interruptLine = IfxCan_InterruptLine_0;
NodeConfig.interruptConfig.traco.priority = 56 ;
NodeConfig.interruptConfig.traco.typeOfService = IfxSrc_Tos_cpu0;
NodeConfig.interruptConfig.busOffStatusEnabled = TRUE;
NodeConfig.interruptConfig.boff = IfxCan_InterruptLine_1;
NodeConfig.interruptConfig.boff.priority = 55;
NodeConfig.interruptConfig.boff.typeOfService = IfxSrc_Tos_cpu0;
If possible pls, share an example for clarity.
Hello, everyone.
I'm currently working on TC334 BOOT related software and I need an area of DSRAM that will not be initialized when the software is reset. I will be putting a section of variables in this area to be used for mutual jump judgments between BOOT and APP. I am currently using tasking's compiler and I don't know if this NO_INIT sector has been requested in the LSL file.
If not, how do I apply it. If so, how do I link the variables to this area.
Thank you!
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/AURIX/TC334-BOOT%E5%BC%80%E5%8F%91/td-p/696063
Show Less各位前輩好,
我現在使用TC387做為馬達控制器的MCU,
現在想要設定6個腳位做為PWM輸出腳位,
但我不曉得該選用哪支腳位做為PWM輸出,
希望能有前輩指導,
謝謝。
Could you provide reference example code for SPI control Master to slave of the multi-select pin configured ?
Able to inject SRI Transaction error, but NOT able to inject when the fault injection is done after the SMU.
Could anybody help with this?
Regards
Show LessHello, recently I am trying to transplant my attitude calculation project to the TC264 microcontroller, which involves a lot of matrix calculations. I saw that TC264 has a DSP. I would like to ask if there are relevant acceleration libraries that can be optimized for tc264 to make the matrix Operations and trigonometric functions have been optimized.I searched illd for a long time and used search engines such as Google. I didn't seem to find a matrix library or a related trigonometric function library. However, I did find an arctangent acceleration function similar to atan2.
Hi ,
I am writing 32 bytes of data into pflash location 0xA013BFE0 or 0xA0133FE0 in TC3735. I am getting error of 97 which is Flashstatus Prog error. Could you please let me know what i am doing wrong.
Thanks
Krishna
Show LessHello Team,
We are working on a project where we are using Infineon TC377 chipset. We would like to have some inputs on how we can access the EMEM memory. We are trying to copy data and then read it from location at EMEM memory range but we are unable to do so.
Additionally, We are also trying to enable OCDS and have performed the required steps but are unable to find any information on the associated register from the data sheet. We are not sure if we have the correct information with us.
We would really appreciate if this can be looked on priority since we have a time constraint in the project.
Please help us out through this. Thank you!
Thanks and regards
Sivaprasath Balachandran
Show Less