AURIX™ Forum Discussions
Hello, recently I am trying to transplant my attitude calculation project to the TC264 microcontroller, which involves a lot of matrix calculations. I saw that TC264 has a DSP. I would like to ask if there are relevant acceleration libraries that can be optimized for tc264 to make the matrix Operations and trigonometric functions have been optimized.I searched illd for a long time and used search engines such as Google. I didn't seem to find a matrix library or a related trigonometric function library. However, I did find an arctangent acceleration function similar to atan2.
Hi ,
I am writing 32 bytes of data into pflash location 0xA013BFE0 or 0xA0133FE0 in TC3735. I am getting error of 97 which is Flashstatus Prog error. Could you please let me know what i am doing wrong.
Thanks
Krishna
Show LessHello Team,
We are working on a project where we are using Infineon TC377 chipset. We would like to have some inputs on how we can access the EMEM memory. We are trying to copy data and then read it from location at EMEM memory range but we are unable to do so.
Additionally, We are also trying to enable OCDS and have performed the required steps but are unable to find any information on the associated register from the data sheet. We are not sure if we have the correct information with us.
We would really appreciate if this can be looked on priority since we have a time constraint in the project.
Please help us out through this. Thank you!
Thanks and regards
Sivaprasath Balachandran
Show LessHi Community,
I've configured UCB_DBG for lock state and provided a password. Now, I need to unlock it. Do I need to reconfigure UCB_DBG (code confirmation) for the default unlock state? If so, could you please provide the detailed steps involved? (I am using TC39 )
Show LessHello All,
I am working on a project where I need to accurately generate a PWM signal with a 50% duty signal with a 1 Hz frequency.
I tried using CCU6 interrupt, GTM (TOM/ATOM), GPT12, and FreeRTOS but all yielded about ~265 us skew per sec as measured by a logical analyzer and a pico-scope.
As per my understanding, the tolerance for the source crystal oscillator is 50 ppm which is equivalent to 50 us per sec, so I aim to stay within this error margin.
How can I achieve such a signal with the latter skew tolerance?
BR,
Amr Khaled
Show LessGood morning,
The version of tricore-gcc provided with ADS is a nice and relatively recent build (11.x) which supports a fair amount of C++20. This is spectacular and useful.
I don't use ADS for anything other than launching winIDEA currently (in a VM), and I'm building our application using standard tools (CMake, Ninja, Ccache) on Linux and sadly I must use wine to use the toolchain. This works, but it's somewhat annoying that there isn't an obvious place to download a Linux release of the toolchain.
Is the source available for tricore-gcc provided by Infineon? Do you have a Linux build that I can request in myICP perhaps? I'm aware that this toolchain not to be used for commercial purposes, and this is entirely fine. I'm working on a publicly funded research project at the moment.
Show LessHello, I want to find a manual for this development board. I checked the similar TC387TFT schematic on this website. Now I have a board with a DIP switch and an adjustable potentiometer. Has it been revised later? I want to find the corresponding manual and schematic. Thank you. The attached picture is my development board, and the PDF is similar to the one I downloaded from the official website
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/AURIX/%E5%AF%BB%E6%B1%82%E8%AF%A5%E5%BC%80%E5%8F%91%E6%9D%BF%E7%9A%84%E5%8E%9F%E7%90%86%E5%9B%BE/td-p/684529
Show LessHi
I would like the BSDL-File for the TC399XX256F300SB for a development for our new product.
Thanks
Dear Community,
I am using A2G TC387 5V TRB S.
I need QSPI pins that only output 3.3V.
The pins P15.5, P15.3, P15.2 (QSPI) output the signals with 5V.
I would also need GPIO pins that only output 3.3V.
best regards,
Patrick
Show LessWhen using the TC23x AB chip, I encountered a problem where SMU reset occurred when writing dFlash.
View errata
1: ALM2 [29] Safety Mechanism: Recovery Timer 0 is enabled by default when powered on.
2: Alarm Configuration The default configuration is SMU_RESET (0b 110-0x6) when powered on
The 2 points above are exactly in line with the description for writing SMU_reset, and some settings SMU_no Action (≠ 0x6)
Understand that the SMU will trigger Reset by mistake,
Question: When the code is actually running, under what circumstances will Unexpected/Unexpected Reset Rejected by SMU Alarms occur?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/AURIX/Aurix-Unexpected-Incorrect-Reset-caused-by-SMU-Alarms/td-p/681480
Show Less