AURIX™ Forum Discussions
text.format{('custom.tabs.no.results')}
Hello All,
I am using Aurix TC399 kit, I am trying to configure some parameters via the command line which is done successfully based on this example https://www.infineon.com/dgdl/Infineon-ASCLIN_Shell_UART_1_KIT_TC397_TFT-Training-v01_02-EN.pdf?fileId=5546d4627883d7e00178a2d656463923
Now I want to have a default configuration applied at startup without the need to send the configuration every time after reset. So is there a way to inject a default command at start-up like simply "info".
BR,
Show LessGreetings!!
We are planning to use Infineon MCU in our project and would like to have the following data for the part - TC387QP160F300SADKXUMA1
1) Schematic & layout guidelines
2) Reference Designs
3) Can we connect ADC & Analog reference alone 5V, VDD=1.25V and other rails 3.3V ?
Hello, Iam getting a CPU context management trap error while debugging _mtcr(CPU_SYSCON,sysconValue.U) in enable_memory_function() .can u please tell me the solution for this issue
Show Less
Hello .I got a CPU context management trap error while debugging enable_memory_protection() function .can u please tell me the solution to resolve this issue.
Show Less
Hi together,
I've tried to import a project, which is developed in BiFaces to the Aurix Studio. The project is a simple gateway beween Ethernet and CAN. Every thing is ok and I can compile the project by the Aurix studio but if I run the project there is no communication over the Ethernet. However it runs when I compile it with the Bifaces. The compiler option and the compiler and Linker are the same.
Can someone help me where the problem is?
Thank you all
Shaham
Show LessHi,
I am using Aurix TC399, in my project I am using around 40 pins as input pins. I need to set interrupt on these pins with edge triggered. I found ERU example code. But I am not able to set all these pins as interrupt pins. Is there any way for configuring interrupt with these GPIOs using ERU?
Or any other way to configure it?
Show LessHi, Can anyone let me know what is the performance class of SAK-TC277T - 64F200S DC AUrix ?? Thanks.
We are able to compile a project using Aurix IDE. We want to create a makefile manually for the same project. While creating the make file, we are getting the below error.
ltc E112: cannot locate 371 section(s):
ltc W141: unresolved reference to "_lc_u_trap_tab"
Microcontroller: AURIX TC233LP
IDE: Aurix Development studio
Compiler: Tasking
we using coomand
Show Less
Based on the official documentation of AUTOSAR, the TC39X is configured as the host for gPTP. When using the underlying EthTSyn driver generated by EB, there are numerous errors in the EthTSyn_Types.h file during compilation, indicating missing semicolons.
After investigating the code, it appears that the errors are related to the undefined definitions of "EthTSyn_IntPortIdxType", "EthTSyn_PhyAddrPtrType", and "ETHTSYN_APPL_VAR".
Show LessI would like to know about the implementation of gPTP in AURIX TC3X7. Is there any support manual for getting to know whether we can implement gPTP in the board.
Any help would be really appreciated here 🙂
Best regards
Rahul
Show Less