Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

AURIX™ Forum Discussions

Sort by:
Vishwa1988
AURIX™
Dear Team, I am Vishwanatha Patel, from VVDN TechnologiesWe would like to buy below metioned evaluation board, i couldn't able find the the same in In... Show More
zhlei327
AURIX™
I am using TC377. I want to copy all functions into RAM and run them. But psram0 only has 64Kbytes, so I have to copy all functions into psram0 and ps... Show More
Anand_501
AURIX™
I need to establish the CAN protocol in the Dev kit. i need CAN Protocol Tx & Rx data transfer sample project Code. #TC234 #kit_AURIX_TC234_TFT #CAN   Show More
Jonson
AURIX™
Infineon Engineers:Hello! I obtained the routine for motor control of TC387 according to Infineon's official link address, which is as follows: Infineon-AURIX_TC3xx_Motor_Control_Application_Kit_TOOL_Instructions_External-UserManual-v01_00-EN.pdf... Show More
Chaabane
AURIX™
Hello all ! I'm evaluating advanced features in the TC275 and need good debugger tool below 200 dollars. Currenly I have kit_aurix_tc275_lite that use... Show More
kikizhang_1980
AURIX™

ECU外部有4路轮速PWM信号输入,MCU是否是通过TIM功能捕捉口读取PWM周期。不知是否合适。

另外一个输入信号是否要单独对应一个TIM单元,也就是说,4路轮速信号需要4个TIM模块,TIM1~3. 是否正确?

FD_aurix
AURIX™
Hi all I've just noticed that not all HWCFG  are exposed on the different derivative. Where can I found some more information on how to handle these d... Show More
explorer357
AURIX™
I use  TC3XX mcal code, when I compiler the project code. Error occurs "error: missing pragma section end for data section 'Config.Cpu0.32bit' ",    i... Show More
Samad
AURIX™
Hi team, We had integrated AURIX TC397x in our Autonomous vehicle. We want to send large amount of data from Linux platform(Jetson device) to AURIX ov... Show More
Amr-khaled-Aziz
AURIX™
Hello All, I am using Aurix TC399 kit, I am trying to configure some parameters via the command line which is done successfully based on this example https://www.infineon.com/dgdl/Infineon-ASCLIN_Shell_UART_1_KIT_TC397_TFT-Training-v01_02-EN.pdf?fileId=5546d4627883d7e00178a2d656463923... Show More
Forum Information

AURIX™

In this forum you can post your questions, comments and feedback about the 32-bit AURIX™ TriCore™ Microcontroller. The AURIX™ offers the highest scalability in performance, memory & peripherals across application. It is a safe and secure companion chip, meeting both the ISO functional safety standards and EVITA full security standards. Here you can also find the links to the latest board pages, SW and Tools GitHub, trainings, documents and FAQs