AURIX™ Forum Discussions
Hello Infineon team,
In all your example codes , you init devices with default configuration values. Then you change some of the values. Can I have what are this initial values in order not to ask for a simple stuffs or to spend a time to find what are defaults?
Show LessHi there,
I'm new to the Infineon hardware and tools. my company just bought the KIT_A2G_TC377_SEC_GTW for a project.
I am trying to run iLLD_TC375_ADS_FreeRTOS_Basic example project on KIT_A2G_TC377_SEC_GTW, when I click Flash&&Start Project I got the following error from console, how can I fix the error and have FreeRTOS running in the board.(I don't need to run the LED app in the example, just trying to go through the process of build FreeRTOS, flash and run)
AURIX Flasher Software Tool 1.0.8.0, built on 2023-07-07 10:18:22 AM
DASWRAPPER::No DUT hardware found
Overall time: 2256 ms
AURIXFlasher Exit Status: Fail
Flashing failed
Hi team
I am trying to config ASCLIN1 with iLLD code ,but there is a question, both the Tx&Rx pin are P15.5。
When I change the Tx pin to P15.4, this channel can't send any data,the same situation occured in ASCLIN0.
I want to know the reason.
Thanks for your reply
Show Lessstatic const IfxAsclin_Lin_Pins lin1_pins = {
.tx = &LIN1_TXD_PIN,
.txMode = IfxPort_OutputMode_pushPull,
.rx = &LIN1_RXD_PIN,
.rxMode = IfxPort_InputMode_pullUp,
.pinDriver = IfxPort_PadDriver_cmosAutomotiveSpeed1
};
void lin_init(uint8 bus)
{
// Initialize one instance of IfxAsclin_Lin_Config with default values
IfxAsclin_Lin_Config linConfig;
IfxAsclin_Lin_initModuleConfig(&linConfig, lin_module[bus]);
linConfig.linMode = IfxAsclin_LinMode_slave;
linConfig.brg.baudrate = lin_baudrate[bus];
linConfig.pins = lin1_pins ;
// Initialize module
IfxAsclin_Lin_initModule(&lin_bus_handle[bus], &linConfig);
}
初始化函数如上,但IfxAsclin_Lin_receiveHeader(&lin_bus_handle[bus], &id);后
lin_bus_handle[bus].acknowledgmentFlags.rxHeaderEnd 标志不为1
参考代码如附件
使用的开发板为TriBoard TC3X7 ADAS TH V2.0 芯片为TC397
Show Less
Hello,
I try to compile an example project for the TC4x Communication board in ADS Limited, but I get the following error
We are aiming to "design in" the Aurix microcontroller for our new Elevator Control project.
For this project, we need to achieve SIL 3 according to the standards IEC-61508.
Could you please advise whether we would require 1 safety core or 2 safety cores to attain this level of safety integrity?
Show LessHi,
I am starting my 1st steps with Aurix, I have downloaded the AurixDevelopment Studio , and SPI_DMA_1_KIT_TC375_LK example from Infineon Code Example Repository.
In the project properties I chanded the Current ToolChain from TASKING to GCC, but When I build the project I get errors
error: #error "Compiler unsupported"
error: #error "Please specify compiler."
error: #error Unsupported compiler.
Why I get Such errors when I try to use gcc "tricore-elf-gcc"?
Show Lesssmartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/AURIX/TC389QP%E7%9A%84%E4%BB%A5%E5%A4%AA%E7%BD%91%E8%AE%BE%E8%AE%A1/td-p/700699
Show Less当前使用 iLLD ASCLIN_LIN_MASTER_1_KIT_TC397_TFT demo例程,直接编译程序刷写后,lin1可以正常发送数据,但是demo中Tx Rx PIN均设置为P15.5,请问这是否有问题,当我把TX pin更改成为P15.4时,数据无法发送,请问这是什么原因
Show Less