AURIX™ Forum Discussions
I use TC3XX mcal code, when I compiler the project code. Error occurs "error: missing pragma section end for data section 'Config.Cpu0.32bit' ", it appear in the picture . How can I solve it?
Show Less
hi could you please share the Safety manual (TC387)for me ?, i can not find it from this website.
thank you in advance .
Using the TC387 chip configuration Autosar OS found that the main core run fly, other cores run normally OS task switching, PC pointer to the _IF_CONST area, D[4] register is 1, D[15] register is 4, according to these two registers with the calculation rules calculated TCN and TIN seems to have problems, in Trap run fly, please ask, what do you have? Ideas recommended?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/AURIX/TC387%E8%B7%91%E9%A3%9E%E5%88%B0IF-CONST/td-p/702834
Show LessI am using the AURIX TC375 litekit. Now, I want to receive data (ADC) and calculate the minimum and maximum value of a 10MHz oscillation and either store the values in a .txt document or output the voltage signal. For this, I need the samling rate to calculate each oscillation. Which example project is the best for realizing this? And can I work with Qt to implement the microcontroller? Thanks in advance.
Show LessHello Infineon team,
In all your example codes , you init devices with default configuration values. Then you change some of the values. Can I have what are this initial values in order not to ask for a simple stuffs or to spend a time to find what are defaults?
Show LessHi there,
I'm new to the Infineon hardware and tools. my company just bought the KIT_A2G_TC377_SEC_GTW for a project.
I am trying to run iLLD_TC375_ADS_FreeRTOS_Basic example project on KIT_A2G_TC377_SEC_GTW, when I click Flash&&Start Project I got the following error from console, how can I fix the error and have FreeRTOS running in the board.(I don't need to run the LED app in the example, just trying to go through the process of build FreeRTOS, flash and run)
AURIX Flasher Software Tool 1.0.8.0, built on 2023-07-07 10:18:22 AM
DASWRAPPER::No DUT hardware found
Overall time: 2256 ms
AURIXFlasher Exit Status: Fail
Flashing failed
Hi team
I am trying to config ASCLIN1 with iLLD code ,but there is a question, both the Tx&Rx pin are P15.5。
When I change the Tx pin to P15.4, this channel can't send any data,the same situation occured in ASCLIN0.
I want to know the reason.
Thanks for your reply
Show Lessstatic const IfxAsclin_Lin_Pins lin1_pins = {
.tx = &LIN1_TXD_PIN,
.txMode = IfxPort_OutputMode_pushPull,
.rx = &LIN1_RXD_PIN,
.rxMode = IfxPort_InputMode_pullUp,
.pinDriver = IfxPort_PadDriver_cmosAutomotiveSpeed1
};
void lin_init(uint8 bus)
{
// Initialize one instance of IfxAsclin_Lin_Config with default values
IfxAsclin_Lin_Config linConfig;
IfxAsclin_Lin_initModuleConfig(&linConfig, lin_module[bus]);
linConfig.linMode = IfxAsclin_LinMode_slave;
linConfig.brg.baudrate = lin_baudrate[bus];
linConfig.pins = lin1_pins ;
// Initialize module
IfxAsclin_Lin_initModule(&lin_bus_handle[bus], &linConfig);
}
初始化函数如上,但IfxAsclin_Lin_receiveHeader(&lin_bus_handle[bus], &id);后
lin_bus_handle[bus].acknowledgmentFlags.rxHeaderEnd 标志不为1
参考代码如附件
使用的开发板为TriBoard TC3X7 ADAS TH V2.0 芯片为TC397
Show Less