Recent discussions
Hi there,
Can HW parity check be used in master mode? From iLLD u can config a master ch to use parity check (<IfxQspi_SpiMaster_ChannelConfig>.parityCheck). But from manual the chapter ch20.8.3 'Parity' is under ch.20.8 'Slave Mode', implying it only work in slave mode.
So if I turn on parity check in master mode (<IfxQspi_SpiMaster_ChannelConfig>.parityCheck = TRUE), will it work?
I am working on TC234.
Thanks for reading, any reply is appreciated
Show Lesshello all,
Can the TC397 sample square waves with frequencies up to 50Mhz and How to configure if possible?
ELF File generation with TASKING Compiler
Hello,
I am working on tc27x Project using TASKING Compiler. Could you help me please generate the .elf file using Cmake .
Kindly share Command for generate .elf file.
Thank you.
Hello. I have MC-ISAR_AS422_TC3xx_CD_2.10.0 package but could find manuals for SENT under user manual folder. Where can I get SENT user manuals?
Show LessI first tried to install :
Infineon-Memtool-DevelopmentTools-v05_00-EN.exe on my windows 10 PC (this installer has been successfully installed else where). After installation, when I first run it, I got pop up "Can't create Memtool user interface !".
Then I downloaded the latest: Infineon-Memtool-DevelopmentTools-v06_00-EN.exe which automatically install pre-requisites. Uninstall the previous version, then install the latest one. I got the same error once I tried to run it.
Please see attached and kindly advise.
Show LessHi,
I would like to check if Multicore instances of MCAL for Aurix TC29x is supported currently ? If so any pointers on how this can be achieved ?
Regards,
Sistla.
Show LessHello! I am using TC234 (PG-TQFP-144-27 Package) for FOC of PMSM. Two AD channels are used for phase current sampling. A confusing problem occurs when testing the AD sampling results with 0 current.
In fact, two hall sensors are used as the current sensors. They offer 2.5V voltage to pin-35 and pin-51 of the chip (configured as AN0 and AN12) with 0 current. The voltage has been tested using oscilloscope, which is quite stable.
If the ADC queue entry immediately leads to a conversion request, the sampling results are stable, as shown in the following picture. The sampling results are 10000 continuous reading results of one ADC channel recorded by an array.
However, some unexpected fluctuations were observed in the ADC sampling results if the ADC queue entry is triggered by GTM.
The difference in register configuration between the two tests are as follows:
Other than this, all hardware and software status are the same. Please help me figure out the reasons. If this problem is not caused by software reasons, please tell me and I will deal with the problem with my hardware engineering.
Thank you very much. Sincerely.
Show Less
I am using GPT12_PWM_Generation_1_KIT_TC375_LK as the base firmware and test the example on my TC37X eval board.
Everything works perfectly.
I then tried to test the incremental encoder feature and I follow the document
iLLD User Documentation Device:TC37A Version: 1.0.1.14.0
|
The example snippet code seems like it carried from version TC2.7.X
◆ TimeConst_1s
#define TimeConst_1s (TimeConst[TIMER_INDEX_1S]) |
time constant equal to 1s
Definition at line 71 of file Ifx_DateTime.c.
Referenced by DateTime_get(), and DateTime_set().
It is clearly has nothing to do with GPT12 module.
May I ask the proper way to get GPT12 module to work, we have to include all the needed defines in different projects?
Does the snippet code in the iLLD document only there as the references or we can use it as closely as possible?
Thank you so much for all of your time and helps.
While trying to flash my TC397 kit , I get this every time. Is there some setting I need to change
"::Loading HEX file ..........
:⚠️ The given program file is trying to write on reserved memory addresses, which will be skipped."
Hello Everyone,
I'm working with TC37x & TC39x controllers and i want to retain the DSPR data over resets.
How to modify the DMU_HF_PROCONRAM register RAMIN value to 0x2[Init_Cold].
I have tried to access with register memory location 0xF804008C. But it's not updating.
Kindly help me.
Thanks in advance.
-Babu Dudekula
Show Less