AURIX™ Forum Discussions
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/AURIX/SAK-TC397XP-256F300S%E5%B0%BE%E7%BC%80BC%E5%92%8CBD%E7%89%88%E6%9C%AC%E6%9C%89%E4%BB%80%E4%B9%88%E5%8C%BA%E5%88%AB/td-p/721501
Show LessUnsure which part of the forum i should post to .. i did have this on the hardware side of things but it may be 'finger trouble'
As it stands at the moment i've adapted the example code using other forum uses 'comments'
i now have 2 nodes , 1 transmit , 1 receive , they are in loop back mode the receive has 2 filters set up. If i transmit from the one node with either of the message ID'd set up in the filter the interrupt goes off plus data is received .. awesome we've made a step forward.
if i turn loop back off and have my can tool connected , i can transmit fine but when i send from my can tool the micro does not respond .
with regards the filtering , i'd like to filter a range of id's but seams i cannot
shed any light people ?
I've tried the code on 2 dev kits so i know it me / code and not hardware.
I've notice some examples start setting base memory address and some don't i've tried both ways with using the addressing the board becomes a 'brick' and i receive a 'trap '.
i'm attching my MCMCAN file , i'm new to infineon so i'm hoping it something i'm not setting or doing (i'm used to dspic / Ti micros) .. any help would be grateful
Thanks,
Show LessHi,
I have a question related to Default Application Memory.
The question: How to know whether DAM is Initialized during startup SW or not?
Thanks.
Show LessCan we use the SPI without interrupts? in polling mode? All examples show only with interrupt. Is there an exmple code. Kindly support !
When AD converting a voltage that is higher than VREF1/2 and lower than the absolute maximum rating, is it guaranteed to capture the maximum value? In other words, if it is 12bitAD, will it be 0x0FFF?
Best Regards,
Tetsuo
Newbie here ,, have been looking at CAN loopback examples (MCMCAN_1_KIT_TC334_LK .... etc etc ) but and i'm happy that it works .. as i can see data in appropriate register for rX. My query is none of the examples show how to transmit a message and/or recieve a message. I've searched the site and found a few "links" but they dont work. Also found a semi worked example - no data on the CAN tool.
If anybody has anything that works or can show me where to look id be gratefull
Cheers
Show Lesswhat is the abbrevation of .epd/.epc file in Mcal context?
Thanks
Greetings Infineon,
Recently we purchased the following evaluation board kits of the AURIX family of MCU:
KIT_AURIX_TC277_TFT
KIT_AURIX_TC297_TFT
Is it possible to get the sources (project) for the demo applications running on these boards?
Thank you,
- G. M.
Show Less