AURIX™ Forum Discussions
Hello,
I have implemented the Lin communication function based on the example " ASCLIN_LIN_Master_1_KIT_TC397_LK", but I found a problem. Because the Lin communication rate is relatively low, I found a problem with the function shown in the following figure. There is a while (asclin->acknowledgmentFlags.rxResponseEnd != 1) function in this interface. It needs to be in a waiting state during operation, which will cause other tasks to be delayed. I want to optimize this interface function. What should I do?
Show Less
Hi,
We are just starting with TC275 and TC377, and ordered following kits : KIT_A2G_TC377_5V_TRB_S, KIT_AURIX_TC275_TRB
Kindly help with below queries:
1) Is there any MATLAB design Toolbox/Aid available for these micro controllers:
If yes
a) Kindly share the links and SOP
b) What are other tools like compilers and debuggers required to design with MATLAB?
c) Is the complete toolchain for MATLAB Design free of cost?
d) Does Toolbox include all peripheral blocks with all possible register settings and flashing/debugging support through MATLAB?
Show LessHi Community,
i'm using the EVADC triggered from the ATOM. According to my understanding the following table is needed to establish an trigger between an Modul and the EVADC.
Is this table editable?
Thanks in advance
Andreas
IfxGtm_Trig.c
Show Less
What's the difference between Triboard with TC39x B-Step (DAS) and Triboard with TC39x A-Step (DAS) in Memtool?
PS:My board is KIT_A2G_TC397_3V3_TFT and my demo projcet is come from Tc397 3v3 5v TFT in ADS.
Show Less
Hello All,
Where can I find the AP32356 ???
Where are store all application notes?
Thanks in advance
Regards
Dear Aurix Eperts,
As stated in 32.12.5 On-Chip Supervision Signals on page 1233 of AURIXTC3XX_um_part2_v2.0.pdf, selecting CH28 as alias for channel 0/1 of any group, the voltage fed through pin AN11 can be read.
I'm trying to use these feature for diagnostic purpose but I always read 0 volt, while selecting CH29-31 I read the correct values stated in Table 264.
Has anyone of you used this feature? Is there a configuration example available to do it?
Thank you very much.
Show LessHello,
Is there any document available that will give a brief understanding of PTA and OVL RAM area for TC2XX series devices?
- Do we have any sample code for filter implementation for M_CAN. And in that code CAN_17_Setfilter like api used or library .
Hi guys,
I am now working with TC397 app kit in Aurix Development Studio;
I found that the procedure can not be stopped at the breakpoint.
Can anyone tell me the reason?
Does the ADS support the breakpoint debug with miniwiggler?
Show Less