AURIX™ Forum Discussions
Where does the program resume when waking up from Standby mode?
For example, in the following program, will it be restarted from func_TestA?
IfxScuWdt_clearSafetyEndinit(IfxScuWdt_getSafetyWatchdogPassword());
IfxScuWdt_clearCpuEndinit(IfxScuWdt_getCpuWatchdogPassword());
--------------- omit -----------------------
MODULE_SCU.PMCSR[0].B.REQSLP = REQUEST_STANDBY;
IfxScuWdt_setSafetyEndinit(IfxScuWdt_getSafetyWatchdogPassword());
IfxScuWdt_setCpuEndinit(IfxScuWdt_getCpuWatchdogPassword());
func_TestA();
func_TestA();
soft_Reset_func();
Show LessHello,
On a TC37x evaluation board, I am trying to write on the PFLASH1 while executing from the CPU0. I can write without any problem on PFLASH0, but writing on PFLASH1 always results in a Data Asynchronous Error. Is there any way to get it working ? Or it is just not possible ?
Thank you,
Ana
Show LessHi.
I use a lot of AURIX MCU and HSM.
I currently need HSM Reset.
I couldn't find any explanation about HSM Reset in manuals.
How can I only reset HSM (Arm Cortex)?
< I already know HOST Reset, I need to reset only HSM>
Thanks
Best Regards
Phillip
Show LessHi,
I have recently started working with TC387 and have been struggling to understand some points regarding the ‘groups’ in EVADC. I have gone through the user manual and the example projects but did not find anything related to the issue in them.
I am looking for some help in understanding the following behavior:
If any channel of a group is configured as a slave conversion source and I want to use the same group (different channel) for another ADC measurement, then this new input must also be configured as a slave source. If I configure the new input as queueMaster then the adc output for the channel configured as slave, reads 0. The valid flag is always 0 for it.
If I change the conversion source for the new input to slave, then both inputs work as expected.
If you need any additional information, please let me know.
Thanks! 😊
Show LessHi All,
I want to configure CAN module in TC399 Micro-Controller,
I want to use same node for transmit and receive, I configured the transmit part, but in reception part i am facing issue,
receive interrupt is not generating, can you share me any example code for this , i want to generate the interrupt for Receive in same node.
Show Less
In the AURIX 2G, there is a register SCU_STCON -- Start-up Configuration Register -- Offset 0xC4.
Bit 15 is STP.
Following sentences are in the User Manual Part 1 Revision 1.4 for STP bit
"
This bit will be always set by FW and can't be reset.
This bit is also cleared by an Application Reset.
STP is automatically set when a shutdown trap occurs.
"
1>
Looks like STP is cleared when Application Reset but during Cold Power On Reset it will be SET.
Is that correct?
2>
FW -- means Boot_ROM Firmware which is SSW
Is that correct?
3>
Can you please point me to documentation regarding "shutdown trap" as mentioned above?
Best Regards Show Less
I would like to understand the following :
The register STCON has access mode as ST, P0. P0 means a master can access it when accen bit is enabled.
1. I have opened the Trace32 and requested a Cold PORST. The execution in Trace32 is now at the start of the bootloader.
2. In this condition, I try to write 0 to this STP bit. But I get SPB bus error meaning the master(CERBERUS) cannot access it. The access enable bit for the master (here CERBERUS) is Enabled in SCU_ACCEN00/10.
If only SSW can write this bit, Why is then the access mode P0 given ? Is it possible to modify the value to 0 at any point ?
Show LessHi.
I bought KIT_AURIX_TC237_TFT because I need to develop hsm solution.
I have read the hsm-startup manual.
And I have understood that hsm bootloader code need to be loaded into hsm code sector first.
But the manual doesn't descrbie how to load the hsm bootloader code.
I guess that i need to use my ude or t32 debugger.
But the KIT cannot be connected with any ude or t32 debugger...
I have already checked host core is connected with debuggers.
I'm in a hurry, right now.
Please help me.
https://www.infineon.com/cms/en/product/evaluation-boards/kit_aurix_tc237_tft/
Thanks
Best Regards
Phillip
Show Less
Hello.
I have a question about Aurix Development Studio.
After install the ADS, I can't debug due to debugger IO error.
So I tried to install the DAS64, but I can not install the DAS64 like below.
But I can not found the DAS64 program and folder in my program folder.
How to uninstall and install the DAS64 program.
Show LessHello, I have some doubts related to Data reduction mode feature of EVADC (32.10.5 Data Modification of Infineon-AURIX_TC3xx_Part2-UserManual-v01_00-EN.pdf). my question exactly how results are being accumulated and what should be expected result after accumulation? can anyone explain the process?
Show Less