AURIX™ Forum Discussions
How is the Can RXFOVPIM hard interrupt configured?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/AURIX/TC389-TC397-%E7%9A%84Can-RXFOVPIM-%E4%B8%AD%E6%96%AD%E5%A6%82%E4%BD%95%E9%85%8D%E7%BD%AE%E4%BD%BF%E7%94%A8/td-p/701282
Show LessHello,
I am using TC23x Aurix microcontroller, I have written a program to receive and transmit the same data(in the same program). But when I am receiving the data, some garbage values is received in the data array. But I can't figure out how to remove these garbage values in the array. So please help with this problem.
Thank you
Show LessHello Infineon,
Greetings for the day!
Problem:
While changing the starting UCB Address of STAD Register of Aurix TC364DP board I have mistakenly changed the password PW0 of BMHD0_ORG. After changing it I am unable to unprotect it again by entering the same password which I entered in PW0 of BMHD0_ORG.
The detailed incident Summary is below:
I have unprotected it by putting 0x00000000 password previously and then mistakenly set the PW0 of BMHD0_ORG to 0x80400000.
But after changing it When I am trying to do unprotect it again. It is showing incorrect password. I am unable to change the UCB address of STAD Register in it.
Can you please suggest how to reset the password so that I can change the UCB Address of STAD Register in Aurix TC364DP?
Could you please assist us on this topic?
Thanks in advance for your support!
I have attached the snippet in attachments.
SAK-TC364DP-64F300F AA
I want to use the SPI communication function of the TC397 chip, due to the PCB design schematic use of the SPI channel all the self-select is occupied, so I need to use the GPIO function to simulate the SPI chip selection, encountered the problem is that the communication occasionally appears to receive the data all the F, I use the hardware chip selection of SPI, SPI initialization need to modify those configurations?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/AURIX/TC39X%E8%8A%AF%E7%89%87-SPI%E4%BD%BF%E7%94%A8%E7%A1%AC%E4%BB%B6%E7%89%87%E9%80%89/td-p/701229
Show LessHello, everyone.
I would like to use the AURIX TC3 in external input clock mode. Referring to the TC3 manual, in section 10.3.1.1 it says to connect the clock source to the XTAL1 pin and leave the XTAL2 pin in high impedance.
In my case, however, the microcontroller is mounted in the Triboard TC3x9, and referring to the Triboard manual, the diagram on page 45 shows the connection of the 20MHz crystal in the two pins XTAL1 and XTAL2.
In my case, I would like to use an external clock with a frequency of 12MHz, and this clock is obtained by means of a square wave signal generator with duty cycle = 50%. The problem is that from the moment I connect the external clock signal to the XTAL1 pin, I don't get the right behaviour of the micro.
At this point I would like to ask the following questions:
1)Does the fact that the 20MHz crystal is connected to the XTAL1 and XTAL2 pins via the board allow an external clock signal to be used?
2)Are there any requirements for the external clock signal? I found from the data sheets that the input frequency must be between 10MHz and 40MHz, while I found nothing about the signal amplitude
Show LessHello,
I am using TC23x Aurix microcontroller, I want to receive data through RX pin and send the same data through TX pin , but the IfxAsclin_Asc_read function is not working , so can anyone please help with this problem(any example code) or have recommendation for using any other function for this.
Thank you
Show LessI am interested in learning about any life cycle risks with using the Aurix TC2xxSAK-TC212L-8F133F AC MCU.
1. How many automotive life cycles has Infineon gone through?
2. How service-proven is it?
3. How much longer is the TC2xx projected to be supported?
4. TC212L8F133FACKXUMA1 vs TC212L8F133FABKXUMA1? There is a major cost difference between these two parts on DKey. ( 448-TC212L8F133FACKXUMA1TR-ND , 448-TC212L8F133FABKXUMA1TR-ND )
Show Less
When I use AURIX Development studio for complile and flash, build is completed, but flashing is failed. The error is in capture. Do you know how can I solve this issue? I do not know what is DUT.
Show Less
How to enable Touch TFT in EVAL TC234 TFT AURIX . Where can I get Video Graphics Library and Example code.
#EVAL TC234 TFT AURIX
#TC234
#Touch
#TFT
#VideoGraphicsLibrary
Show Less