AURIX™ Forum Discussions
Hi,
I have Configured and Tested TLF35584 with TC399 with Window Watchdog enabled in NORMAL mode, its working fine with Watchdog getting its periodic trigger at WDI PIN. and CAN module was developed and tested separately. But while I Integrated CAN Module with TLF35584 Code, CAN module is not working. What could be the reason.
Show LessCan we build .s file (Assembly source file) by using Aurix Development Studio?
Need peak soldering temperature for SAL-TC364DP-64F300F AA. Kindly help me to get that?
Hi,
I am new to developing with AURIX MCUs and tried to build a small application that reads data from a SPI Slave and Communicates to a PC via Ethernet. I've managed to get the examples for SPI over ASCLIN and the Ethernet example based on LwIP running fine.
Now I've ported the example into a new application with Core 0 handeling the SPI via ASCLIN2 and the Ethernet Echo example running on Core 2. For SPI Baudrates above 8.4Mbit/s this works perfectly fine, however for slower Baudrates the Ethernet is not responding and the LED on the Connector stays off. It seems like the instruction txData->U = *data++; of the Methode IfxAsclin_write8 causes this behaviour.
Does anyone has a Idea what could cause this? From my limited understanding of the Architecture, the use of the SPB should be the only intersection between Core 0 running SPI and Core 2 managing the GETH and using the debugger shows that the arbiter should use a round robin scheme to manage transfers.
Thanks for your help!
Max
Show LessGreetings,
I am new to using Infineon Aurix TC375 Lite Kit. I would like to know if I can set up the tools, libraries/frameworks for the Aurix TC375 Lite Kit for Linux Ubuntu. As far as I know, I did not find steps on how to set up the environment for Linux. I did find the Developer Center Launcher for Linux but really could not find any guide or tutorial for Linux to do the initial setup. It would be helpful if I can get an answer on whether or not it is possible/recommended to use Linux for Aurix TC375 Lite Kit. And also some links or guidance on how to set up the development environment for Linux.
Thank you.
Kind Regards,
Ram
Show LessHI:
I need some help on how to setup Aurix Studio to work with custom board(our sample board based on TC277 Applicate Kit reference board).
I tried flash the board I got following error message :
Unhandled Exception: System.IO.FileNotFoundException: Could not load file or assembly 'System, Version=4.0.0.0, Culture=neutral, PublicKeyToken=b77a5c561934e089' or one of its dependencies. The system cannot find the file specified.
at AurixFlasher.Program.Main(String[] args)
Flashing failed
For Debugging, the following Error message came out:
Starting Debugger...
The debug instrument IO could not be initialized.
The GDI debug instrument provided the following error message.
An internal error has occurred.
Using Debug Target Configuration:
Target: Generic Infineon AURIX Board
Selected CPU type: tc27xd
Register file: C:/Infineon/AURIX-Studio-1.9.0/plugins/com.tasking.ctc.debug.win32.x86_64_1.12.14.0/ctc/include/sfr/regtc27xd.xml
Communication: Universal Debug Access Server
Debug Instrument Module: gdi2mcdtc
Using Flash Configuration:
Monitor : C:\Infineon\AURIX-Studio-1.9.0\plugins\com.tasking.ctc.debug.win32.x86_64_1.12.14.0\ctc\etc\ftc27x.sre
Workspace address : 0x70000000
Number of devices : 5
Sector buffer size : 8192
Device 0:
Address : 0xA0000000,0x80000000
Vendor : Infineon
Chip : TC2_4560k
Subname : Program Flash 0
Width : 32
Size : 2097152
Number of chips : 1
Unused address lines : 0
Device 1:
Address : 0xA0200000,0x80200000
Vendor : Infineon
Chip : TC2_4560k
Subname : Program Flash 1
Width : 32
Size : 2097152
Number of chips : 1
Unused address lines : 0
Device 2:
Address : 0xAF000000
Vendor : Infineon
Chip : TC2_4560k
Subname : Data Flash Bank 0a
Width : 32
Size : 393216
Number of chips : 1
Unused address lines : 0
Device 3:
Address : 0xAF100000
Vendor : Infineon
Chip : TC2_4560k
Subname : Data Flash Bank 0b
Width : 32
Size : 16384
Number of chips : 1
Unused address lines : 0
Device 4:
Address : 0xAF110000
Vendor : Infineon
Chip : TC2_4560k
Subname : Data Flash Bank 1
Width : 32
Size : 65536
Number of chips : 1
Unused address lines : 0
Configuration: TC27xD
Starting Debugger...
The debug instrument IO could not be initialized.
The GDI debug instrument provided the following error message.
An internal error has occurred.
How to configure or setup Aurix Studio project to get around this problem?
Thank you
James
Show LessHi,
I have a sensor connected at analog pin AN3 of TC389QP-160 Evaluation board whose values are being read using EVADC Group0 Channel 3 and result register at EVADC_G0RESD2.
I am not able to monitor the converted values from Sensor in Trace32 watch window. On checking at EVADC result register, it is always zero. The observation is same for other configured analog pins through EB-tresos . However, DIO pins are working properly for both of the input/output configurations.
I am not sure about whether that is a hardware pin issue or EVADC is not working. I would first like to analyze if there is an issue with EVADC on the hardware board.
There seems to be no issue with the software as same software is working fine on other TC389QP-160 board and the sensor values from EVADC can be monitored properly.
Please suggest some ways to debug the EVADC issue.
Show LessHello,
i would like to ask for help regarding debug interface lock (software implementation) on Aurix litekit 275 .
Debug lock was implemented according to AP32389 application note. Debug interface is locked successfully, however we can not unlock it. We were using memtool.
I would like to ask for help regarding unlocking device what should i try to unlock it. I read almost all forum topics regarding similar issue.
Also is there any known issues when implementing interface lock with code and unlocking it with memtool?
Error code i receive.
Any kind of advise, response would be appreciated.
Regards,
Jan
Show Less
Hello,
I am using a SAL-TC377TP-96F300S AA device. Can you please clarify if AMU.LMU_DAM functional block is available in this device ?
I went through the AURIX TC37x User Manual and Appendix and there is no reference/mention of AMU.LMU_DAM block anywhere.
SM is the only documentation which says The AMU.LMU_DAM main purpose is to provide two high-performance ASC modelling units, however it is not clear if TC377TP device has these units or not.
Appreciate any feedback on this topic
Show Less