AURIX™ Forum Discussions
I make the project for hsm and tricore separately.
and I run to build the project for tricore like tc397.
In case of 1. there is not error when build
case 1.
{
mau = 8;
size = 3M;
type = rom;
map cached (dest=bus:sri, dest_offset=0x80000000, size=3M);
map not_cached (dest=bus:sri, dest_offset=0xa0000000, reserved, size=3M);
}
But In case of 2. the error happens like ltc E821: ["..\Lcf_Tasking.lsl" 998/61] syntax error: absolute location in memory for group does not map to space mpe:vtc:abs18.
"640K" means the size of hsm
case 2.
{
mau = 8;
size = 3M-640k;
type = rom;
map cached (dest=bus:sri, dest_offset=0x800A0000, size=3M-640k);
map not_cached (dest=bus:sri, dest_offset=0xa00A0000, reserved, size=3M-640k);
}
What should I do to resolve this issue?
Hi,
We observed that XRAM Content is cleared during system wake-up from standby mode. Warm power on reset or Cold power on reset will clear the XRAM memory?
Show LessHi, I want to switch to user mode in tc39x. I tried to change the IO bit of psw register but it always setting the interrupt stack control bit(IS) bit. I even tried to change it through an isr in this case the register value isn't changing at all(the isr executes other instructions like toggling gpr value). One reply I got is to change the register value through upper context save area but at that memory location I cant find the psw values. I dont know if I am seeing it correct or wrong . What should I do?
Show LessHello. Infienon team
here are my 2 question.
Q1.
I'm using TC364DP MCU and also using TLE5012B Motor position sensor.
I'm trying to communicate with SSC protocol, it doesn't workl well.
And i'm using ILLD example code, but i can't find SSC example in ILLD.
i think MPS and MCU are both infineon product, so i think there is sample code.
can you give sample code? help me.
Q2.
If you doesn't have TLE5012's ILLD code or sample code, i have anther question.
I implemented communication via QSPI ILLD module.
But SSC's protocol is different to SPI communication, so i can't get exact data.
i want to know how QSPI module works.
here is my question.
If QSPI module's RX pin get data and RX buffer is filled, then RX ISR is called even though QSPI module doesn't work?
the topology is below picture. MCU's MOSI and MISO is connected to same node(P6111) .
so, when i try to communicate via ILLD QSPI module, my sending command is returned via nodeP6111. i don't know how to implement via ILLD QSPI module.
can you help me to implement SSC communication via QSPI ILLD module?
thank you.
Show Less
Anybody found any of the cad files for this demo board?
1. Step 3D model
2. Layout files
3. native schematic files
Hello dear Infineon:
A test application and a UDS CAN boot were implemented. (ADS V1.8, TC367 EvtKit -5v)
The issue is:
if the debugger is started from ADSV1.8, the SW can jump into App from boot, and the App runs well.
If the debugger is not started (only plug the power supply), the App seems run into trap (no LED is on)
I guess there is something wrong in the UCB.
The UCB part are all same for Boot and App (two Apps- simple Led and BSW)
Could you please give me some hint?
And I found even in App tasking lcl, the entry of CPU0 and CPU1 are changed,
#define LCF_STARTPTR_CPU0 0x80020000
#define LCF_STARTPTR_CPU1 0x80304100
but in UCB, the entry address is still 0xA0000000 for both Boot and App.
The hex file and lcl file are attached for your reference.
thanks and BR
Zhou Yi
The
Show Less
Error:
"C:\\app\\TASKING\\TriCore v6.3r1\\ctc\\bin\\amk" -j12 all
Linking to RN050524-S1-Bootloader-Mainline.elf
ltc F014: core mpe:tc0 specified on commandline not found in LSL file
amk E452: ["makefile" 68/0] target 'RN050524-S1-Bootloader-Mainline.elf' returned exit code 1
amk E451: make stopped
please suggest me how to resolve this error.
Show LessHI ALL:
Problem Description: The project is switched from boot to app. If different MO is used in app and boot for the same ID, message in app fail to be received.
I was hoping to Deinit CANFD in boot, but I failed. Expected solution
Thanks
Show LessHi Community,
I want to generate an interrupt using a high priority message (FRAME or CAN signal with specific ID), I followed the steps that are defined in the user manual .
the problem is that I get an interrupt when receiving all the frames sent on the bus, not a specific can frame
I followed this step to config canfilter and interrupt
• At least one Standard Message ID Filter Element is configured with priority
flag set (S0.SFEC = “100”/”101”/”110”)
• No Extended Message ID Filter Element configured
• Non-matching extended frames are accepted (GFC.ANFE = “00”/”01”)
The HPM interrupt flag IR.HPM is set erroneously on reception of a non-highpriority extended message under the following conditions:
1. A standard HPM frame is received, and accepted by a filter with priority flag
set
--> Interrupt flag IR.HPM is set as expected
2. Next an extended frame is received and accepted because of GFC.ANFE
configuration
--> Interrupt flag IR.HPM is set erroneously
Hi, why does the IO bit in PSW register wont change, other bits get changed why is this happening