Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

AURIX™ Forum Discussions

tnallusamy
AURIX™
Hello Team, I walk through the TC375XX tricore infineon Micro safety manual, I see lot of internal and external software and hardware safety mechanism... Show More
MelonSoda
AURIX™
Hello. I'm using Tricore TC37x and TC36x.From what I understand, Tricore suspends its watchdog timer when OCDS debugger is attatched.What I'm curious ... Show More
alexsohn
AURIX™
Hello, we are trying to extend the example code https://www.infineon.com/dgdlc/en?dcId=8a8181663431cb50013431cb500b0000&downloadTitle=mcd_demo_basic_120412.zip&download=L2RnZGwvbWNkX2RlbW9fYmFzaWNfMTIwNDEyLnppcD9maWxlSWQ9ZGIzYTMwNDMxZWQxZDdiMjAxMWY0NjlhYzQwZTU2YWY=... Show More
Jack_gao
AURIX™
If VEVRSB of TC387 is connected to QST of TLF35584, and VEXT is connected to QUC, TLF35584 enters sleep mode when hibernating, and QST and QUC output ... Show More
wangchenyu
AURIX™
tc3xx LMU
solved msg Solved
hi could anyone tell me if the LMU data will be reset after Mcu was reset by TC35584? or which memory area can keep unchanged after reset by 35584 apa... Show More
franky2215
AURIX™
HI, we are working on a project where it requires to use the hypervisor on TC387 board, over that multiple vms(suggest an os iam thinking to install a... Show More
fgallo
AURIX™
Hi, I'm using CAN timestamp configured as @Kavya_B suggested in other topic. It is configured to 1us resolution and it is driven by a GTM timer. I'm s... Show More
explorer357
AURIX™
TC387配合TJA1145/FD收发器使用的问题,使用EB配置Spi为同步模式,发现无法唤醒这个Can收发器,有没有有经验的高手指点一下有什么配置参数要求吗,目前我是把收发器WAKE脚拉高,然后用SPI把收发器寄存器Mode Control 设置为normal,但是我似乎用spi读取不到正确的数据... Show More
晚秋
AURIX™
  hi : I met a compiler error when using hithtec llvm to compiler the demo pjt .it is a demo pjt build in Tasking but I do not have the smartcode lic... Show More
fgallo
AURIX™
Hi, I have 4 nodes of a can module configured and connected to the same can bus. I'm saving timestamp as @Kavya_B suggested me (tick resolution 1us, d... Show More
Forum Information

AURIX™

In this forum you can post your questions, comments and feedback about the 32-bit AURIX™ TriCore™ Microcontroller. The AURIX™ offers the highest scalability in performance, memory & peripherals across application. It is a safe and secure companion chip, meeting both the ISO functional safety standards and EVITA full security standards. Here you can also find the links to the latest board pages, SW and Tools GitHub, trainings, documents and FAQs