AURIX™ Forum Discussions
Hello,
I am using TC366DP. On the Ethernet interface when there is a burst of traffic or multple streams sending data to the processor, the ethernet interface becomes nonfunctional. When I say nofunctional it means no packets make it to the processor.
I have narrowed this down to interrupt not being triggered by RX DMA channel to the CPU Core 0.
Wondering if anyone else has seen this problem and resolved it.
Thanks!
Show LessHi there,
In my software development, I have a use case where the external variable is defined in one partition and accessed and cleared in other partitions. As a result, the controller is going into a memory protection trap.
I'm working with a TC36X microcontroller.
Please share your thoughts to resolve the issue.
Thanks
Show Less
Referring to "https://community.infineon.com/t5/AURIX/Create-complementary-pwm-with-IfxGtm-Atom-PwmHl-driver/td-p/319495"
Can I configure,
#define PWM0 IfxGtm_ATOM1_1N_TOUT72_P15_1_OUT // LED0
#define CCX0 IfxGtm_ATOM1_3_TOUT71_P15_0_OUT
#define COUTX0 IfxGtm_ATOM1_1N_TOUT72_P15_1_OUT // LED0
#define PWM0_OUTPUT NULL_PTR // Use DTM for output signal
#define PWM1 IfxGtm_ATOM1_2N_TOUT73_P15_2_OUT // LED1
#define CCX1 IfxGtm_ATOM1_6_TOUT74_P15_3_OUT
#define COUTX1 IfxGtm_ATOM1_2N_TOUT73_P15_2_OUT T // LED1
#define PWM1_OUTPUT NULL_PTR // Use DTM for output signal
Hello team,
Currently i am facing new issue, while configuring DMA with daisy chain for 4 channels.
please find the configuration details
Getting interrupt from EVADC G2CH4 result event and configured DMA Channel 96 for it.
And requirement is to measure 4 EVADC channel details by use of daisy chain method, for that i have configured immediate 3 low priority channels to record the other EVADC channel results.
Following DMA channels are configured as daisy chain to fill 64 x 4 (word) circular buffer
DMA Ch 96 - daisy chain
DMA ch 95 - daisy
DMA ch 94 -daisy
DMA ch 93 - HW trigger
for this above configuration, i only get first two rows of data in circular buffer.
do we need RROAT or TREL to keep TSR.CH bit pending to execute remaining rows of circular buffer ?
And during start of data transfer , i can see the address like
after 6rows of update or it exceeds 0x300 address, then immediately it goes to 0x200 address
here i need 32 rows to update.
My configuration is given below for DMA CH96
DMA CH 95
Could anyone support me to find the solution for this ?
Show Less
Hello to all. I am a electrical engeener, I work mostly with automotive electronic modules ( repair, clone, adaptation) In my work I find more and more the TC2xx based mcu. I found on official site memtool software and miniwiggler. Is that enough to READ and WRITE the TC2xx? I found around the web DAS Interface for this type of mcu, but no info about DAS Interface here in official site. Please help with advice what soft and hardware I will need to work with this MCU family?
Show LessHello All,
I have recently purchased KIT_A2G_TC397XA_3V3_TFT eval board and was trying to run the blinky LED code that comes as a sample code.
But to my surprise it did not work.
The Application Kit Manual for TC3X7 shows that P13.0 to P13.3 are connected to LED and the sample code is also written in the similar way. But actually P33.1 to P33.4 are connected to the LED.
Now I am confused that are there more such mismatch between the Application Kit manual and actual board?
I have attached the Application kit manual and the documentation for the sample code.
Please let me knwo if anyone has an updated Application kit manual or have faced similar issue.
Thanks in advance.
Show LessHi,
I've got a TC377 board (specifically KIT_A2G_TC377_5V_TFT - Infineon Technologies), and when it was new it came with some demo software that used the display and had a lot of different functionalities. I was thinking that I could learn a lot from fiddling around with the source code for that.
I think I've managed to find the software here: Home - Microcontrollers / AURIX Customer Documentation (infineon.com)) (need to register to access it).
I'm assuming the correct version for my board is the "Application_Kit_TC377_V1.0.0.zip".
But I've run in to some trouble trying to compile & flash the software with Aurix Development Studio. I'm thinking that maybe I'm doing something wrong when importing the project. So far I've tried to just select the folder and import the whole thing (does not work).
Secondly I tried to create a new project for my board, and then just copy the source files. This does not work either, or rather, after making tons of changes in order to get everything to compile, I can flash it but it does not run as I remember it (display not working etc.).
So I'm wondering if anyone has tried and succeeded in getting this demo software to run?
Thanks
Show LessHi Community,
In AURIXTC3XX_um_part1_v2.0.pdf,
Figure 165,The formula in the red box is shown below
About this formula, I don't understand “concatenate(SMU_FSP.TFSP_HIGH,SMU_FSP.TFSP_LOW)”.Does that mean taking the value between SMU_FSP.TFSP_HIGH and SMU_FSP.TFSP_LOW?
Show LessDoes AURIX ILLD have the typedef of Std_ReturnType? It is in AUTOSAR MCAL base.