AURIX™ Forum Discussions
Anyone have sample code for implementing functional watchdog in tlf35584
Hello all,
i am using TIM5 of TC387 with 200Mhz frequency for PWM duty cyle measurement.
but during measurement i can see it is working in 100Mhz.
i can see cluster 0 to 4 can be work in 200Mhz and cluster 5 to 8 can be work with 100Mhz
can any one confirm my understanding is correct ?
Show Less
Greetings,
Im trying to change the memory layout of my board TC397 such that the DLMU locations that are set as:
9000 0000H - 9000 FFFFH 64 Kbyte LMU (CPU0 DLMU)
9001 0000H - 9001 FFFFH 64 Kbyte LMU (CPU1 DLMU)
9002 0000H - 9002 FFFFH 64 Kbyte LMU (CPU2 DLMU)
9003 0000H - 9003 FFFFH 64 Kbyte LMU (CPU3 DLMU)
To
9000 0000H - 9002 FFFFH 192 Kbyte LMU (CPU0 DLMU) (accessible only through CPU0)
9003 0000H - 9003 FFFFH 64 Kbyte LMU (CPU3 DLMU)
I did make the changes in the linker file as-well as the bus access group
Is there something else that I am missing as I haven't been able to get the required results.
Best Regards
Show LessHI,
I had some problems communicating with flaxray using TC375
The following is the configuration of the frame header. It is normal to configure communication in this way.
ID: 8 Can send data to another controller
ID:9 Indicates that data of another controller can be received
Below I have modified MessageBuffers = 8
so that the controller cannot send or receive data
May I ask what went wrong with my configuration and how to modify it?
Show Less
Hello Support team,
What does it mean when the flag Unexpected Configuration Error in Status Register is set?
what problems can activate this flag ?
thanks and best regards
Show LessWhether the SBAB Buffer full error is a critical error? How can we get the Criticality of SMU Alarms ?
As per my understanding, the SBAB Record can be cleared using FLASHCON2 register. So, if the alarm is triggered for the error, the error can be cleared using FLASHCON2 register, right? Or reset is required?
Show LessHello,
We are using Tasking compiler with ETAS OS and the TC397 B Step Microcontroller.
We are facing a linker error as below.
We saw a similar error from Tasking: TCVX-44101 Definition of a trap service routine causes a linker error even if the default handler is disabled
These are our current startup configurations for each core
We are stuck as to how to resolve this error.
Could you please help us with the resolution for this.
Thanks,
Satya Praneeth
Show LessHi,
We are using SAKTC364 microcontroller and TLF35584 PMIC in our project. What can be the minimum and maximum SPI clock frequency, to be configured into software to establish a communication between the controller and peripheral.
Show LessHi,
We are using TC377 to generate PWMs in Master Slave Fashion.
TRIGOUT bit is used to link the PWMs. However, we had a query if PWMs fall on different ATOM, is it possible to link them?
For example 1 channel in ATOM 1 is Master and channels in ATOM 3 &4 are slaves?
Show Less