Recent discussions
Hi everyone,
I have a trouble related to TC397 starterkit ver2.
Today my board is always on reset (ESR0 led is always RED ON). I think it always in reset state.
I can't flash any new software from AURIX Developement Studio.
I have already also refer the post https://community.infineon.com/t5/AURIX-Development-Studio/TC387-starter-kit-board-always-in-reset/m-p/336664
How can I solved the problem now?
Thank you guy
Sang
Show Less
Hello,
I've just installed aurixide_1.7.2_Windows_x64.exe and I can see that DAS 7.3.7 was also installed(installer in AURIX Development Studio install dir) but it does not work. Trying to flash a project results in an error
Aurix Flasher 2.5.3.0, built on 3/17/2022 3:12:47 PM
DASWRAPPER::ERROR init DAS API. Do you have DAS drivers installed?
Overall time: 123 ms
AurixFlasher Exit Status: Fail
DAS struct not initialized
Flashing failed
But DAS is installed, just that it does not work. -> see attached picture.
I've tried with reboots and reinstalls but to no avail.
Thanks for the help,
George
PS1: If I install DAS_V7.1.8 it works, but when trying to start a debug session a popup informs me that DAS 7.3.7 is needed.
PS2: Windows 10 X64
PS3: I have a TC334 Lite Kit
Show LessHello,
I tried to flash the TC38x microcontroller ECU and it failed but now I am unable to communicate/connect or flash the TC38x with the Infineon MEMTOOL via MiniWiggler. I think the TC38x target is locked, as I can see an error as IF_LCK . Can you let me know how to unlock the target device. I am thinking probably I should reset the microcontroller but cannot find the right procedure.
This is the error message:
MEMTOOL Error messages:
Controller0.Core0.Tc2CoreTargIntf: Can't connect target !
Controller0.Core0.Tc2CoreTargIntf: Can't connect target device via DAS !
Hi, I used the TC397 Core0 and Core1 to run our application, Core0 for main application, Core1 for peripheral control.
My problem is, when I tried to call the reset function "IfxScuRcu_performReset(IfxScuRcu_ResetType_application,0x0000)" at Core0, it will stuck at Core0 initial step.
Any comment or suggestion will be appreciated.
Show LessHi I,m using tc275 (Hightec compiler )and I have this error:
.bmhd_1 loaded at [80020000,8002001f] overlaps section .text
Any suggestions?
Thanks
Show Less
We are using the TC277TP ECU for our program. we flashed the CBL & SBL using Lauterbach debugger, and Application software using CANoe.
After first time flashing the CAN communications were observed. However, when we tried to reflash the ECU it started giving error of "Debug Port Failed". And after this we are not able to connect to the ECU using JTAG/DAP.
Please help to resolve this error.
Show Lesshello. i'm using TC 364 DP and trying to flash software to mcu, but below error happen.
please help me to solve this problem. And i run DAS device scanner program, and attach my current status as screen shot.
i think mini wiggler can't detect MCU, and i don't know why this happen.
1. i'm using mini wiggler JTAG/DAP/SPD V2.0
and when i try to flash current project, below error message is happen.
------------------------------------
Aurix Flasher 2.5.3.0, built on 2022-03-17 오후 10:12:47
DASWRAPPER::No ECF hardware found
Overall time: 413 ms
AurixFlasher Exit Status: Fail
Flashing failed
------------------------------------
i checked my device management, and my computer acknowledge mini wiggler.
when i try to debugging, below error message is happened.
-------------------------------------
2. The debug instrument IO could not be initialized.
The GDI debug instrument provided the following error message.
An internal error has occurred.
-------------------------------------
Using Debug Target Configuration:
Target: Generic Infineon AURIX Board
Selected CPU type: tc36x
Register file: C:/Infineon/AURIX-Studio-1.6.0/plugins/com.tasking.ctc.debug.win32.x86_64_1.12.14.0/ctc/include/sfr/regtc36x.xml
Communication: Universal Debug Access Server
Debug Instrument Module: gdi2mcdtc
Using Flash Configuration:
Monitor : C:\Infineon\AURIX-Studio-1.6.0\plugins\com.tasking.ctc.debug.win32.x86_64_1.12.14.0\ctc\etc\ftc36x.sre
Workspace address : 0x70000000
Number of devices : 6
Sector buffer size : 8192
Device 0:
Address : 0xA0000000,0x80000000
Vendor : Infineon
Chip : TC3_6616k
Subname : Program Flash 0
Width : 32
Size : 3145728
Number of chips : 1
Unused address lines : 0
Device 1:
Address : 0xA0300000,0x80300000
Vendor : Infineon
Chip : TC3_6616k
Subname : Program Flash 1
Width : 32
Size : 3145728
Number of chips : 1
Unused address lines : 0
Device 2:
Address : 0xAF000000
Vendor : Infineon
Chip : TC3_6616k
Subname : Data Flash 0
Width : 32
Size : 262144
Number of chips : 1
Unused address lines : 0
Device 3:
Address : 0xAF400000
Vendor : Infineon
Chip : TC3_6616k
Subname : Data Flash UCB
Width : 32
Size : 24576
Number of chips : 1
Unused address lines : 0
Device 4:
Address : 0xAF800000
Vendor : Infineon
Chip : TC3_6616k
Subname : Data Flash CFS
Width : 32
Size : 65536
Number of chips : 1
Unused address lines : 0
Device 5:
Address : 0xAFC00000
Vendor : Infineon
Chip : TC3_6616k
Subname : Data Flash 1
Width : 32
Size : 131072
Number of chips : 1
Unused address lines : 0
Configuration: TC36x
Starting Debugger...
The debug instrument IO could not be initialized.
The GDI debug instrument provided the following error message.
An internal error has occurred.
Re-loading 'D:\Test Software\AURIX-v1.6.0-workspace\IDB_2p0_PLOCK_M_v3_copy\Debug\IDB_2p0_PLOCK_M_v3_copy.elf'...
Using Debug Target Configuration:
Target: Generic Infineon AURIX Board
Selected CPU type: tc36x
Register file: C:/Infineon/AURIX-Studio-1.6.0/plugins/com.tasking.ctc.debug.win32.x86_64_1.12.14.0/ctc/include/sfr/regtc36x.xml
Communication: Universal Debug Access Server
Debug Instrument Module: gdi2mcdtc
Using Flash Configuration:
Monitor : C:\Infineon\AURIX-Studio-1.6.0\plugins\com.tasking.ctc.debug.win32.x86_64_1.12.14.0\ctc\etc\ftc36x.sre
Workspace address : 0x70000000
Number of devices : 6
Sector buffer size : 8192
Device 0:
Address : 0xA0000000,0x80000000
Vendor : Infineon
Chip : TC3_6616k
Subname : Program Flash 0
Width : 32
Size : 3145728
Number of chips : 1
Unused address lines : 0
Device 1:
Address : 0xA0300000,0x80300000
Vendor : Infineon
Chip : TC3_6616k
Subname : Program Flash 1
Width : 32
Size : 3145728
Number of chips : 1
Unused address lines : 0
Device 2:
Address : 0xAF000000
Vendor : Infineon
Chip : TC3_6616k
Subname : Data Flash 0
Width : 32
Size : 262144
Number of chips : 1
Unused address lines : 0
Device 3:
Address : 0xAF400000
Vendor : Infineon
Chip : TC3_6616k
Subname : Data Flash UCB
Width : 32
Size : 24576
Number of chips : 1
Unused address lines : 0
Device 4:
Address : 0xAF800000
Vendor : Infineon
Chip : TC3_6616k
Subname : Data Flash CFS
Width : 32
Size : 65536
Number of chips : 1
Unused address lines : 0
Device 5:
Address : 0xAFC00000
Vendor : Infineon
Chip : TC3_6616k
Subname : Data Flash 1
Width : 32
Size : 131072
Number of chips : 1
Unused address lines : 0
Configuration: TC36x
Starting Debugger...
Using Debug Target Configuration:
Target: Generic Infineon AURIX Board
Selected CPU type: tc36x
Register file: C:/Infineon/AURIX-Studio-1.6.0/plugins/com.tasking.ctc.debug.win32.x86_64_1.12.14.0/ctc/include/sfr/regtc36x.xml
Communication: Universal Debug Access Server
Debug Instrument Module: gdi2mcdtc
Using Flash Configuration:
Monitor : C:\Infineon\AURIX-Studio-1.6.0\plugins\com.tasking.ctc.debug.win32.x86_64_1.12.14.0\ctc\etc\ftc36x.sre
Workspace address : 0x70000000
Number of devices : 6
Sector buffer size : 8192
Device 0:
Address : 0xA0000000,0x80000000
Vendor : Infineon
Chip : TC3_6616k
Subname : Program Flash 0
Width : 32
Size : 3145728
Number of chips : 1
Unused address lines : 0
Device 1:
Address : 0xA0300000,0x80300000
Vendor : Infineon
Chip : TC3_6616k
Subname : Program Flash 1
Width : 32
Size : 3145728
Number of chips : 1
Unused address lines : 0
Device 2:
Address : 0xAF000000
Vendor : Infineon
Chip : TC3_6616k
Subname : Data Flash 0
Width : 32
Size : 262144
Number of chips : 1
Unused address lines : 0
Device 3:
Address : 0xAF400000
Vendor : Infineon
Chip : TC3_6616k
Subname : Data Flash UCB
Width : 32
Size : 24576
Number of chips : 1
Unused address lines : 0
Device 4:
Address : 0xAF800000
Vendor : Infineon
Chip : TC3_6616k
Subname : Data Flash CFS
Width : 32
Size : 65536
Number of chips : 1
Unused address lines : 0
Device 5:
Address : 0xAFC00000
Vendor : Infineon
Chip : TC3_6616k
Subname : Data Flash 1
Width : 32
Size : 131072
Number of chips : 1
Unused address lines : 0
Configuration: TC36x
Starting Debugger...
The debug instrument IO could not be initialized.
The GDI debug instrument provided the following error message.
Connection error between client and server
The debug instrument IO could not be initialized.
The GDI debug instrument provided the following error message.
An internal error has occurred.
Using Debug Target Configuration:
Target: Generic Infineon AURIX Board
Selected CPU type: tc36x
Register file: C:/Infineon/AURIX-Studio-1.6.0/plugins/com.tasking.ctc.debug.win32.x86_64_1.12.14.0/ctc/include/sfr/regtc36x.xml
Communication: Universal Debug Access Server
Debug Instrument Module: gdi2mcdtc
Using Flash Configuration:
Monitor : C:\Infineon\AURIX-Studio-1.6.0\plugins\com.tasking.ctc.debug.win32.x86_64_1.12.14.0\ctc\etc\ftc36x.sre
Workspace address : 0x70000000
Number of devices : 6
Sector buffer size : 8192
Device 0:
Address : 0xA0000000,0x80000000
Vendor : Infineon
Chip : TC3_6616k
Subname : Program Flash 0
Width : 32
Size : 3145728
Number of chips : 1
Unused address lines : 0
Device 1:
Address : 0xA0300000,0x80300000
Vendor : Infineon
Chip : TC3_6616k
Subname : Program Flash 1
Width : 32
Size : 3145728
Number of chips : 1
Unused address lines : 0
Device 2:
Address : 0xAF000000
Vendor : Infineon
Chip : TC3_6616k
Subname : Data Flash 0
Width : 32
Size : 262144
Number of chips : 1
Unused address lines : 0
Device 3:
Address : 0xAF400000
Vendor : Infineon
Chip : TC3_6616k
Subname : Data Flash UCB
Width : 32
Size : 24576
Number of chips : 1
Unused address lines : 0
Device 4:
Address : 0xAF800000
Vendor : Infineon
Chip : TC3_6616k
Subname : Data Flash CFS
Width : 32
Size : 65536
Number of chips : 1
Unused address lines : 0
Device 5:
Address : 0xAFC00000
Vendor : Infineon
Chip : TC3_6616k
Subname : Data Flash 1
Width : 32
Size : 131072
Number of chips : 1
Unused address lines : 0
Configuration: TC36x
Starting Debugger...
The debug instrument IO could not be initialized.
The GDI debug instrument provided the following error message.
An internal error has occurred.
Using Debug Target Configuration:
Target: Generic Infineon AURIX Board
Selected CPU type: tc36x
Register file: C:/Infineon/AURIX-Studio-1.6.0/plugins/com.tasking.ctc.debug.win32.x86_64_1.12.14.0/ctc/include/sfr/regtc36x.xml
Communication: Universal Debug Access Server
Debug Instrument Module: gdi2mcdtc
Using Flash Configuration:
Monitor : C:\Infineon\AURIX-Studio-1.6.0\plugins\com.tasking.ctc.debug.win32.x86_64_1.12.14.0\ctc\etc\ftc36x.sre
Workspace address : 0x70000000
Number of devices : 6
Sector buffer size : 8192
Device 0:
Address : 0xA0000000,0x80000000
Vendor : Infineon
Chip : TC3_6616k
Subname : Program Flash 0
Width : 32
Size : 3145728
Number of chips : 1
Unused address lines : 0
Device 1:
Address : 0xA0300000,0x80300000
Vendor : Infineon
Chip : TC3_6616k
Subname : Program Flash 1
Width : 32
Size : 3145728
Number of chips : 1
Unused address lines : 0
Device 2:
Address : 0xAF000000
Vendor : Infineon
Chip : TC3_6616k
Subname : Data Flash 0
Width : 32
Size : 262144
Number of chips : 1
Unused address lines : 0
Device 3:
Address : 0xAF400000
Vendor : Infineon
Chip : TC3_6616k
Subname : Data Flash UCB
Width : 32
Size : 24576
Number of chips : 1
Unused address lines : 0
Device 4:
Address : 0xAF800000
Vendor : Infineon
Chip : TC3_6616k
Subname : Data Flash CFS
Width : 32
Size : 65536
Number of chips : 1
Unused address lines : 0
Device 5:
Address : 0xAFC00000
Vendor : Infineon
Chip : TC3_6616k
Subname : Data Flash 1
Width : 32
Size : 131072
Number of chips : 1
Unused address lines : 0
Configuration: TC36x
Starting Debugger...
The debug instrument IO could not be initialized.
The GDI debug instrument provided the following error message.
An internal error has occurred.
Now, I have a controller based on the TC1728. And I want to know which compiler supports this microcontroller.
I have already downloaded and installed the ADS. But the ADS doesn't support the microcontroller.
And I want to know where to get the example of that microcontroller.
Can you help me with this aspect? thank you.
Show Lessis it possible to config an interrupt on start receive after 2[ms] delay time,
or is it any other possible way to
find a start or end of a frame with known size and known delay time between frames.
Dears, Hello,
My first post.
I have just started working on TC387 5V TRB A2G kit.
It seems that there are several code examples for iLLD for this target but I am not able to find them.
I found "chm" for iLLD but it does not work also (I can just open it but nothing can be displayed afterward).
I'm looking for some software developer guide or something which can help me to understand the iLLD and other drivers for example, for 5V_TRB evalboard please.
I looked a lot around but I couldn't find any. Any help would be greatly appreciated!
below screenshot of the chm for iLLD which is not working.
Examples found only for the TFT version (nothing for the TRB):
Thanks!
Akd