AURIX™ Forum Discussions
Value of STMEM3 as example after Cold power on reset is A0F3FB1F in user manual but while debugging it's value 0x80f3ff1f
problem in bit 10 which must be reserved 1 , and bit 29 which indicate Flashcon1 register check is started
how i solve problem of reserved bit and how start Flashcon1 register check ?
Show Less
I want to implement FreeRTOS on the TC389 board. But I don't know what folders should be included and how to struct the AURIX Project. Please help me..
Show LessAURIXtc33x
we found this but we need more clarification for example :
we need to test the MC1 (SFI F2S ) and MC2 (CPU0) , so how we can inject non correctable error for them ?
or there is another way to inject the fault for them to be able to test their interrupt .
Show LessHello
I'm trying to figure out Aurix's internal sensors.
I presumably found registers that I need to access, which are 'DTSCSTAT' and 'DTSSTAT'. So i've got their offsets but I dont quite get what is the base address of the periphery which they belong to.
The periphery is *Power Management System (PMS)*
and somehow it has two base addresses.
F0240000 with no note. or
F0248000 whit the note 'FPI slave interface'
Which one should I use? Or could you point out to the place where the FPI is described in detail?
Thank you!
Hi, We want to generate a fast ticks of 10us via timer. It is the highest priority timer. However, we tried it via GPT but we noticed the ticks are missing randomly.
Kindly let us know if GPT method used is correct or if we can generate and ISR /tick via PWM Module (Period is 10us) is better.
Show LessHi Community,
In AURIX_TC3xx_Part2-UserManual-v02_00-EN.pdf,
Figure 467, ECONz (z=0-7).CPH = 0 is used when communicating with a slave that delivers a valid value of the first bit immediately after being selected with an SLS signal. In such a case the first clock edge in a frame is used to latch the first bit. The second edge delivers the second bit value.
I do not understand the meaning of the second bit value, is the 2nd edge red marked edge?
Does it deliver the first data bit latched at the first edge of the same pulse?
Thanks
Show Less
Hi everyone,
I'm wondering if you have an official example code.
And I have an additional question. I am considering making a Line Tracer development training video using TC275 LITE KIT in Korea.
The reason is that there are not enough various videos to learn about using the AURIX chip.
There are not enough videos in Korea for new developers to enter and learn.
I'm trying to create and share it from a personal developer's point of view, not from a corporate level, but I'm wondering if there's any problem.
By default, you want to use ADS, which Infineon provides for free.
Thank you.
Show LessI'm working with TC377T, when I tried to change the mode of cannode to STARTED, the CCCRi.INIT was set to NORMAL, but the PSRi.ACT was still in SYNCHRONIZING . it was supposed to be IDLE. I checked with the Baud rate setting and clock setting , they are all correctly setted.
Any thoughts on what might be going on ?
Show LessHello,
I am using Aurix TC397XX, can I use some of the ADC pins as GPIs instead of ADC channels since some of them have port numbers?
For Example:
Show Less