AURIX™ Forum Discussions
I am working in EDSADC of TC37X controller.
How should the full-scale value of main CIC filter be calculated here?
Is there any formula or is it directly defined by the bitfield GAINCALx.CALTARGET? If yes, how is the value of bitfield GAINCALx.CALTARGET calculated?
Show LessHi,
I am developing flash bootloader for Tc387. So I integrated the flash demo code Flash_Programming_1_KIT_TC375_LK available in ADS .I started with Erase and I get trap SBE 1 for program flash but data flash is ok.
I have disabled core1 to 3 as shown below
Below is the code with sectorAdder being 0xA00E0000. The copyFunctionsToPSPR() is done in the calling functon.
The Trap I get is as below
DEADD is having SBCU address and not sure why it is pointing to it.
Please help to fix it.
Thanks,
Show Less
Hello,
is there an example of UDP socket that works on TC397?
Please, reply.
Hi infineon's team
I designed a tc397 MCU as the main board of the main control chip and used P00.8 as the ADC input. When the input voltage was high, the ADC value was incorrect. When the input voltage was 4.85V, the voltage of the pin was only 4.077V measured by the voltmeter, and the result was abnormal. Is the maximum effective voltage of P00.8 as ADC input VDDM?
Thanks
Show Less
Hello All,
I have seen a pretty wiered behaviour on TC397XA 3V3 evaluation board.
When ever I try to send Data on CAN bus, data is only visible on CANL, CANH remains always high.
This is the same case for Rx.
I connected logic analyser on the controller's Tx and Rx pin and saw that Data is being correctly fed to TLE9251VSJ. (Screenshot of logic analyzer attached)
Show Less
Hello,everyone!I wrote the bootloader using the TC234 chip, but after the boot jumped to the app, the main loop could run, but without interrupting. Someone can resolve this, thank you!
Show LessWhen I try to validate MCU configuration by using tresos as third party integration in DaVinci configurator tool with MC-ISAR_AS42x_TC3xx_BASIC_1.40.0-rc I get following error:
MCU01803: Invalid XPath-expression for Attribute "RANGE" of node "/AUTOSAR/TOP-LEVEL-PACKAGES/ActiveEcuC/ELEMENTS/Mcu/McuModuleConfiguration/GtmGlobalConfiguration/GtmGlobalConfiguration/GtmTomGlobalConf/GtmTomGlobalConf/GtmTomChannelConf/GtmTomChannelConf_6/GtmTimerPortPinSelect": (1806) The XPath-expression "ecu:list(concat('Gtm.','Tom',substring-before(substring-after(node:fallback('->node:path(.)','GtmTomGlobalConf_BMD/GtmTomChannelConf'),'GtmTomGlobalConf_'),'/GtmTomChannelConf'),'Channel',substring-before(substring-after(node:fallback('->node:path(.)',''),'GtmTomChannelConf_'),'/GtmTimer'),'ToutSel'))" caused an error: (35010) The requested ECU resource property "Gtm.TomChannel6ToutSel" does not exist
Is it a known issue? Any suggestion for solving this issue? Show Less
TC3xxシリーズでのDAP over CAN Messages (DXCM)機能の使用方法をご教授頂けないでしょうか。AURIX_OCDS_um_v2.9.1.pdfにはTC2xxシリーズでの説明があるのでこちらのTC3xx向けのものがあるようでしたら提供していただきたいと考えております。
Show Less