AURIX™ Forum Discussions
As shown in the attached photo, TC364 has a Vflex pin (136) in the LQFP package and is not in the QFP package.
1. SAK-TC364DP-64F300F AA(TQFP-144)
<Datasheet>
=>Looking at the data sheet contents, the QFP package thinks that the VFLEX supply is internally connected to the VEXT supply, so If VEXT=5V, is VFLEX=5V / If VEXT=3.3V, is VFLEX=3.3V.
2. SAK-TC364DP-64F300W AA(LQFP-144)
<errata sheet>
=> The LQFP package requires the VFLEX supply to be connected externally, which of the following configurations is correct?
a) Like the QFP package, If VEXT=5V, is VFLEX=5V / If VEXT=3.3V, is VFLEX=3.3V possible?
b) If VEXT=5V, is VFLEX=5V or 3.3V / If VEXT=3.3V, is VFLEX=5V or 3.3V possible?
Thanks~
Show Less
I want to reset counter of tom's channel (ex. Tom1's Channl 1) from trigger of another tom channel(ex. Tome0's channel 1)'s trigger signal.(trigger signal is generated when Tom0's channel's pwm rising edge timing)
I'm trying to use illd functions to do above reset from triggering.
What illd function should I use?
Is there any similar questions like mine or code example for this problem?
Show LessHello,
I have applied for a free evaluation of aurix tc38xq, but it is not possible to create a new Irq module. Is this situation normal?
Regards,
jackp0t
Show LessPlease help me to flash & debug the elf or hex file using tasking toolset eclipse ide. I'm using miniwiggler.
could you please explain what is BIFACES and how to use it?
Thanks!
Lucas
#8042000 12172
I created simple C/C++ "Hello World" project but it didn't compile at all having this error message.
Kindly check the attachements
Error: An internal error occured during : "FetchJob".
Show Lesswe are using SAK-TC397XA-256F300S BD Powered from TLF35584QVHS2.
1. When we connect the supply 12 V at input of the PMIC we see the outputs generated but all these supplies along with POR signals pulses after 600ms for 20ms low. Which we think it is something to do with INIT timer.
2. So, to bypass this, we Pulled the MPS pin of TLF35584QVHS2 to high 5V so that we can use the Microcontroller Programming support feature. And I can see the Supplies and the POR is stable and Not Pulsing now.
However, when we try to flash the controller using DAP interface (Mini wiggler) with MPS held high (5V). We still see the programming failed. Attaching the logs here…
Below is the error message when MPS is pulled low:
Aurix Flasher 2.5.3.0, built on 3/17/2022 6:42:47 PM
Connected to device... [TRICORE] DAS JDS miniWiggler V3.1
::Loading HEX file ..........
:⚠️ The given program file is trying to write on reserved memory addresses, which will be skipped.
Overall time: 770 ms
AurixFlasher Exit Status: Fail
Flashing failed
Error message when MPS is pulled high:
Aurix Flasher 2.5.3.0, built on 3/17/2022 6:42:47 PM
Connected to device... [TRICORE] DAS JDS miniWiggler V3.1
::Loading HEX file ..........
:⚠️ The given program file is trying to write on reserved memory addresses, which will be skipped.
::Erasing Flash memory .......... (Pass)
::Programming Flash memory .......... (Pass)
AurixFlasher - DAS::Error: Device reset could not be performed.
Overall time: 3168 ms
AurixFlasher Exit Status: Fail
Flashing failed
The same code works on EVM KIT_A2G_TC397_3V3_TFT. let me know if we are missing something.
Hi,
We are using AURIX SAK-TC364DP-64F300W AA MCU.
To interface analog voltage, we used RC filter between opamp output & MCU.
Are the following only points to be considered to interface with ADC?
1. Cut off frequency to be considered while calculating the RC values.
2. ADC sink current should be limited as per datasheet limits.
3. ADC sampling frequency should be at least twice the highest input signal frequency (Nyquist theorem).
Any other points that need to be considered while calculating the RC values to interface ADC of AURIX?
Regards,
Abhishek D.
Show Less
Hello,
I am trying to integrate support for the AURIX TC375 into my current custom build system which uses makefiles to compile my project code. I have been unable to use the TASKING compiler outside of the IDE. Are there any suggestions as to how I should approach this problem, and / or which compilers I should use?
Thank you!
Show LessHi,
My bootloader run debug mode in ADS(aurix development studio) with miniwiggler is work good, but run in normal mode always fail at download app step, seems MCU no any response in this phase, have any advice?
Thanks.
Supplementary Note:
CanRxPin:IfxMultican_RXD0A_P02_1_IN
CanTxPin:IfxMultican_TXD0_P02_0_OUT
External HardWare pin, HWCFG[3:4:5]=[0:1:1]