AURIX™ Forum Discussions
text.format{('custom.tabs.no.results')}
Hi Vector,
I am working on a project using pclp V2.0 to test our code base which contains both C and C++ code.
Is there available a pclp (lint-nt) lint file for use with the tricore gcc compiler? For example, for other gcc compilers it is named co-gcc.lnt etc.
Its version are as follows.
tricore-gcc v4.9.4
tricore-g++ v4.9.4
Regards
Farmer Jo
Show Less
Hi,
We are using Triboard TC387 Eval board for evaluation to one of the projects. We are seeing some issue and we need support to resolve the same.
The board was working, and I did flash, debug multiple times before three weeks (approx.).
And yesterday we tried to connect to the board and flash but it shows the below error:
“ DASWRAPPER:: No ECF hardware found “.
And we did probe the ESR0, PORST and ESR1 lines on the working board and non- working board.
Port also not detected in device manager.
Please find attached all the screenshots for your reference.
Also, the RST led always ON.
Please let me know if you need any information and advise how we resolve the issue.
Thanks in advance.
Show LessHello, everyone. I would like some help on how to read and locate the trigger position in the registers.
Let me explain: I have written a code where a PWM is generated from TOM 0 channel 13 to be used as a trigger for EVADC Group 0 channel 0.
As a trigger output I have to use ADC Trigger 0, and this can be guessed from the manual.
What I don't understand is why I have to use Trigger Source 15 when I configure the EVADC.
Why? How do I understand this from the manual? Can you help me, please? Because if I want to use other TOM or ATOM modules I want to be able to recognise the trigger source from the manual.
Could it be that for the board I am using the manual I am looking at is wrong? I am using a SAL-TC399XX-256 F300S-BD.
Thank you in advance.
We would like to use the miniwiggler for debugging Aurix TC33x based porject.
We are using an external build toolchain which uses the tasking compiler to build the automotive application. We have several iSystem debuggers that we are currently using for flashing and debugging.
Our company purchased Miniwiggler devices that we would like to use for the same purpuse. We understood that the Miniwiggler can be used with Aurix Development studio. But when we tried to setup a project in it, we could not find a project wizzar to configure the environment for debugging purposes only. So this means we would like to flash the elf files and also include the project files in the IDE so that we are able to browse the code and set breakpoints, etc.
Is it possible ?
To setup the Aurix Development studio so that it builds the code is beyond our scope. We just want to use the tool for debugging.
hi,
i use the Aurix Development Studio developping a TC275 project,
1、i have a problem ,my bootloader start 3 core and cpu0 cpu1 cpu2 are run ok, have any bug;
but ,when jump to app ,it only run cpu0 ,the cpu1 and cpu2 are stop,
and i am sure i have call the "(void)IfxCpu_startCore(&MODULE_CPU1, (uint32)&_Core1_start);" and
"(void)IfxCpu_startCore(&MODULE_CPU2, (uint32)&_Core2_start);"both in boot and app.
but cpu1 and cpu2 not start in app,only run in boot;
2、And then ,i try to stop cpu1 and cpu2 in boot, i modify the define:
compile the project ,it have err
these two question make me wondering. could you help me ?
thanks much
Show Less
Good morning,
I am realizing through ATOM channels PWMS with up down counters but they are not synchronized between them.
The first one started after the second one (about 50 ns) and I don't know why ( I am using the same code and same clock and same CNO=0 initial value for both counters).
Can you help me?
Exist a way to do center alignment of pwms with up down counters? Which bits I have to set?
Thank you in advance.
Show LessHello,
I have done the following configuration for main CIC filter of DSADC in TC37X controller.
DICFG.DSS = ONCHIP_MOD
GAINCAL.CALTARGET = 0x3FFF
FCFGC.CFMDF = 0x27
GAINCORR.CICSHIFT = 17
GAINCORR.GAINFACTOR = 6038(Resulting factor : 1.474)
GAINCAL.CALFACTOR = 4096(Resulting factor : 1)
GAINCTR.CICDEC = 512
GAINCTR.GAINFACTOR = 5897
GAINCTR.CICSHIFT = 28
DICFG.ITRMODE = Bypassed
OFFCOMP.OFFSET = FFF8
and I am getting the result(RESM) as 16372 when the input voltage is 5V. I am not able to understand how this result(RESM) value is got.
My understanding about CIC shifting. The value of GAINCORR.CICSHIFT is 17, which means the bits 17-33 of CIC filter output will be considered. But here the result is only 16 bits(GAINCAL.CALTARGET) long, then how will this extraction be done?
My understanding on how the result value is evaluated. Once the extraction is done based on shifter(CICSHIFT), then it will be multiplied by GAINCORR.GAINFACTOR(during normal operation) and then multiplied by GAINCAL.CALFACTOR. Then finally it will get subtracted by offset value to get the result(here integrator is disabled).
Is my above understanding correct?
Also can anyone let me know how the result(RESM) is obtained.
Thank you
Show Less
Hi,
Does anybody know how to connect an interrupt handler to the interrupt vector table? For example, how would one connect the ISR (EXT_INTP_CH28_CAT2_ISR)?
Thanks
Show Less