AURIX™ Forum Discussions
Hi,
We are working on TC297 triboard, I need schematics for this product. I couldn't see any document at https://myicp.infineon.com/ and at any other place. I wonder about is there any one who can succeed to access this document. I dont know why it is very difficult to get sch. I don't know how to go on. Can someone help me?
Show LessHello,
I am using in my project TC377TP with iLLD. The main application is running in core_0. In core_1 I want to execute some computations when the ADC result is valid in core_0 using interrupt event. If I use core_1 I get the following error. In core_0 or core_2 is running well.
/* Function to init channel and interrupt */
void initEVADCChannelG1_PH1(void)
{
/* Create channel configuration */
IfxEvadc_Adc_ChannelConfig adcChannelConfigG1_PH1;
/* Initialize the configuration with default values */
IfxEvadc_Adc_initChannelConfig(&adcChannelConfigG1_PH1, &g_adcGroup1_PH1);
/* Select the channel ID and the respective result register */
adcChannelConfigG1_PH1.channelId = (IfxEvadc_ChannelId)(V_OUT);
adcChannelConfigG1_PH1.resultRegister = (IfxEvadc_ChannelResult)(V_OUT);
adcChannelConfigG1_PH1.resultServProvider = IfxSrc_Tos_cpu1;
adcChannelConfigG1_PH1.resultSrcNr = IfxEvadc_SrcNr_group1;
adcChannelConfigG1_PH1.resultPriority = 100;
/* Initialize the channel */
IfxEvadc_Adc_initChannel(&g_adcChannelG1_PH1, &adcChannelConfigG1_PH1);
}
Show Less
hi,sir:
请问TC397 EVB KIT_A2G_TC397_5V_TFT EVB 自带的系统中是否包含RTOS?能否提供此EVB对应的SDK开发包?
多谢!
Good evening.
I work with the Aurix TС298TP processor in conjunction with the DAR Miniwiggler 3. I use the DAS software and memtool. The connection was made by Jitag. The Das program defined the infinion tricore family. Next, I need to enter a code to access the processor and further work. The problem is that the programming of the P flash processor was not successful. The processor is now in BOOT mode. There is a file with information P flash, it was previously read by a third-party programmer. Tell me how you can find out the password to access the processor and make a record to restore work.
My KIT_A2G_TC357TA_3V3_TRB board cannot power on.
When plug in power, following 3 LEDs blinked very briefly and then stay off:
- D504 RST (red) -> RESET LED indicate the reset state of the board (/ESR0)
- D506 +3V3 (green) -> +3,3V power supply indication
- D507 +5V (green) -> +5V power supply indication
The board power supply on X501 stays at 12V all the time.
I notice the "Failsafe handling" section in board manual, so I tried pressing ENA button (S502).
With each button press, said 3 LEDs blink very briefly just like power on.
Press and hold the button makes no difference.
Closing jumper JP501 as mentioned in the manual also makes no difference.
When pressing the ENA button (S502), I can see a very brief 3.3V signal on the closed jumper pin with oscilloscope, as shown in following picture:
If I connect the board's USB to PC, I can see the "Infineon DAS JDS COM" and "Infineon DAS JDS Debug" in windows device manager.
However, if I try to debug my code with ADS-limited, it shows following error:
Starting Debugger...
The debug instrument IO could not be initialized.
The GDI debug instrument provided the following error message.
An internal error has occurred.
Please advise.
Show LessI want to run RGMII + rtl8211f on TC377TP with Aurix 1.9.4, so I copy ethernet module from Ethernet_1_KIT_TC397_TFT, the board has the same pin mappings as demo, but I get GETH_MAC_PHYIF_CONTROL_STATUS == 0 & GETH_GPCTL == 0. Only MDIO can read PHY register, tx & rx fail.
Also I tried MAC loopback with GethConfig.mac.loopbackMode = IfxGeth_LoopbackMode_enable; GETH_MAC_PHYIF_CONTROL_STATUS is still 0
Show LessHello
I need to know the information on how to enable the QSPI0 and QSPI1.
Is it possible to enable these communication, which are the registers that are used.
I looked at GLOBALCON register. however, there is no information on how to enable QSPI 0, QSPI 1 individually.
With Regards
Hemanth
Show LessAfter importing example project (e.g. ADC_Filtering_1_KIT_TC375_LK) in ADS-limited, how can I change the device to program it to my Triboard TC357TA eval-kit?
Show LessIs there any OS support for Tricore MCU?
Such as FreeRTOS, ucOS, ROS, etc..
Hi,
Does the micro onboard the KIT_A2G_TC375_LITE dev-kit come with an integrated HSM? If not is there a recommended dev-kit with the TC375 chip?
Show Less