AURIX™ Forum Discussions
Hello,
I would like to know if anyone in the community has experience with TC367 and MAX24288.
Wondering if anyone has experience issues with the RGMII interface with MAX24288 or any other PHY chip.
Thanks!
Show LessHi,
In Infineon-AURIX_TC3xx_Part1-UserManual-v02_00-EN.pdf, the VDDPD voltage range provided in table 290 is conflicting with the voltage range provided in Figure 113, Table 284 and Table 285. Please confirm the correct voltage range of supply voltage VDDPD.
Table 290: 1.125V -1.375V
Table 284: 1.15V - 1.43V
Table 285: 1.15V - 1.43V
Figure 113: 1.15V - 1.43V, PREOVVAL range: 1.43V – 1.48V, PREUVVAL range: 1.1V – 1.15V
Best Regards,
Hyma Varghese
If the software implemented for the ED device is run on the PD device by mistake, how will it affect the microcontroller?
Could the microcontroller be destroyed?
We are using TC27x/37x microcontroller.
Show LessHi team,
Please address my following queries which will help me a lot for further proceedings.
What is default start-up mode of AURIX TC397x when the device is delivered from the factory?
How to change BMHD contents to configure the start-up mode as ASC Generic Bootstrap? I am aware what are the changes to be done in BMHD to select ASC generic Bootstrap loader mode, but how to apply the changed BMHD into AURIX?
BMHD verification and start-up mode selection code flow is explained in user manual, can I have a programmatic(code) fro the same please?
In ASC bootstrap loader, target needs some inputs from host like baud rate setting, ack ect, Can I have some reference codes to design such host application to implement ASC BSL?
Help is most appreciated.
Regards,
Shafi.
Show Less
Hello,
I wanted to know the pull-up value when the GPIO is in tri-state mode.
If my understanding is wrong could you please explain the internal working of a GPIO in tri state mode.
I am using Aurix TC397XX.
Thanks
Show Less我尝试将cpu0,1,2的寄存器FLASH1的MASKUECC和寄存器FLASH2的ECCCORDIS均设置为1,但是读取PFI ECC Registers
(ECC Status Register)寄存器值为0xA800A8(参照TC3XX用户手册第一部分.pdf的546/1881)任然错误,请问有方法解决吗?
BR
jack
Show LessHello,I have been using ADS for a while now and can't debug with ADS recently. My colleague can use the burster to debug the program, so exclude the board or burster failure factors.
The problems that arise during Debug are shown in the figure.
Chip: TC275
I have been worried about this for a long time. I hope to get your help or advice. Thank you.
Show LessHello all,
I have working on a project based on TC397B, while I am building the project without compiling the default [cstart.c]and [cstart_tcx.c] and depending on linking on with them directly from tasking library the the software is starting successfully without any problem, but when I tried to build [cstart.c]and [cstart_tcx.c] files in my project the software doesn't starting successfully [some cores are freeze].
My question is there any option to get the cstart files that tasking are using to create their library or how can I configure the startup paramters in cstart.h file.
Thanks in advance
Hello,
I am interested in uploading an executable .out file that has been generated outside of the IDE to my target device. How would one go about doing this using the AURIX Development Studio or HighTec IDE?
Hardware used is the AURIX TC375 Lite Kit.
Thank you!
Show Less