AURIX™ Forum Discussions
Hi,
I've just picked up Aurix Development Studio and Infineon products more generally - in terms of normal CAN_FD usage, should a user be able to stick fairly rigidly to the functions declared in MCMCAN_FD.h?
Thanks,
Show Less
Hi,
We are using TC387 but most of the examples are given for TC397 which we can't directly run in our board. Is there any easy way to convert projects of TC397 to TC387?
Show LessI am trying to configure an Infineon Aurix TC334 Lite kit QSPI as master. So far, I managed to configure the necessary pins, change the polarity to work with Gyro 6 Click Gyroscope (bit order - MSB, sampling edge - riging). I using an SPI sniffler and as far as i can see data is being transmitted but i receive nothing on MISO. Do you have any idea?
I've attached a snip with the SPI MOSI/MISO and the code as well.
Show Less
Hello community, Are there in Simulink/Simscape actual models or examples where a simulation with an AURIX-Processor is supported without the actual hardware (no HiL)?
Show LessI'm facing an issue in Aurix Development Studio where including certain functions (AppInit()
, blinkLED()
, NvmInit()
) prevents the execution of runShellInterface()
. However, commenting out these functions allows runShellInterface()
to execute normally.
- Affected Functions:
AppInit()
,blinkLED()
,NvmInit()
. - Expected Behavior: After executing these functions,
runShellInterface()
should execute. - Observed Behavior:
runShellInterface()
doesn't execute when the mentioned functions are included. - Debugging Attempts: Tried debugging tools but couldn't identify the cause.
Hello,
Target device is the TC333LP. The Mbist component follows all the principles and instructions written in the AURIXTC3XX_ts_part1_V2.5.1. The initialization process and running the NDT of GANGs 0, 2, 3 gives positive results and is working without any issues. The situation changes when we want to initialize DSPR SRAMS of the CPU0 (DMEM and DMEM1).
Enabling the test mode using the MEMTEST registers results in the bus error. The situation is the same for DMEM and DMEM1 and they use different MEMTEST registers. The initialization was done in compliance with hints given in the Handling of Large DSPR SRAMs chapter in the TC33xEXT_appx_um_v2.0 document - the test mode for them is not running parallelly.
It does not also seem like an access mode issue - the registers change their values to those which are written into them. The autoinitialization is also not running when the test mode is enabled.
What I have found is that the Data Integrity Error in the Scratchpad memory.
How can this issue be addressed? What could be the reason of it?
Hello, I have a problem and need to be supported 🙂
Problem:
We use PWM to control the motor and the PWM duty will be updated by ISR every 125ms and we don’t want to change the ISR schedule.
Now the project uses P02.0 and TOM1CH8 for PWM output generation and the frequency is 62.5ms but we don’t want the next PWM cycle duty is kept.
So the idea is: we want to use 2 PWM outs in the P02.0 pin - TOM0CH8 and TOM1CH8. is it possible to have 2 outputs in a 1 pin.
Show Less
Hello,everyone,I have a KIT_AURIX_TC297_TFT evaluation board, I have programmed UART_VCOM_1_KIT_TC297_TFT demo into it, follow Infineon-AURIX_TFT_Training-v01_00- EN.pdf file says that when I connect the evaluation board to the PC through the USB cable, I should be able to connect the evaluation board to the PC through the USB cable. UART_VCOM_1_KIT_TC297_TFT-Training-v01_00- EN.pdf file says that when I connect the evaluation board to the PC through the USB cable, I should be able to to see a serial port on the PC, set the serial port baud rate to 115200, and I should be able to receive hello world information from the evaluation board. But I can't see anything on my PC right now, what is the problem? Thank you.
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/AURIX/UART-VCOM-1-KIT-TC297-TFT-demo-not-work/td-p/479019
Show LessWe would like to know if Infineon TC399 SDK has any software library support for PMSM motor speed control? For example, are there any libraries that provide api for pid, park and clark transform functions?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/AURIX/TC399/td-p/475437
Show LessHow can I sample a channel using DMA, and I interrupt the channel to dma, so that all channels of a group will trigger DMA move, but I only want one channel of the group to trigger DMA move, for example, group 8 channel 14 triggers DMA move, but group 8 channel 1 does not trigger DMA move
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/AURIX/A-channel-such-as-G8CH14-is-acquired-using-DMA/td-p/476281
Show Less