AURIX™ Forum Discussions
Hi,
We have the Vehicle CAN at P20.7(RX)/P20.8(TX) and using the Triboard Tc387 for the time being. When looking at the below table I dont see the P20.7 RXD as can wakeup pin. Does it mean that I need to change my VCAN to P14.1(RX)/P14.0 or is there any other way to stick with P20.7?
Also I have the below SCR files but scr_wcan.h is missing. Please help me on this scr_wcan demo files?
Thanks,
Show Less
Hello AURIX Support team,
Currently, I'm working with VADC_Module of TC234 AURIX Tri-Core. My application is required to use all 16 analog channels (from pins AN0 -> AN15).
I'm using the ADC Aurix Example to test the ADC conversion.
I've modified the Channel_ID parameter to switch to different Channel_ID one by one. I've also observed the respective registers in debug mode.
The problem is when the value VADC_BRSSEL0 reached Channel 11, it automatically reseted to 0 in the next run, and nothing happens when "channel" variable run from ID_12 to ID_15 (VADC_BRSSEL0 = 0 in these cases). Then everything went back to normal when the "channel" variable reset back to ID_0.
I've also found some relating information regarding the VADC_BRSSEL0 register in TC234 Reference manual. Is it meant that I need to switch the Converter Group (G0 and G1) to use MAXIMUM 24 analog channels (not count 2 additional channels)? If yes, how could I configure using the same structure as AURIX example?
Thank you very much!
Show LessHello,
I have 2 projects ( bootloader and app ) for TC275 and want to flash both with debug symboles.
IDE gets stuck at this stage
I setup the app project like it is showing in the picture
I used to set it up in STM32CueIDE but not sure how in AURIX IDE
Please advice on how this can be acheived
Show Less
hello
i am working on project where i am using AurixTc375LK.
I need the information on how can i get SIP for the controller?
Do i need to pay any cost for that or is it free?
Show LessWe have selected TC375TP96F300WAALXU MCU for the development, Any pinout tool suggestion (Similar like XMC pinout tool)will be useful for pin mapping.
Show LessHi Infineon Expert:
I currently using the official Infineon iLLD library code, the QSPI polling method takes about 10us to read, I want to find a QSPI operation code based on register operations to improve the reading speed, please support, thank you!
Show LessIs there a KIT_AURIX_TC223_TRB EVM design circuit diagram? OR-CAD, PADS, Altium etc. Only PDF files. I think having a circuit diagram would help us develop it
Show Less在使用TC387时,我配置一个中断,产生中断请求后,到对应的回调函数,而到了DefaultInterruptHandler中,有哪些情况会进DefaultInterruptHandler中吗,我在 UM 中看到了这几种,是否还有其他的可能性(end customer :小米汽车)
Show Less