AURIX™ Forum Discussions
text.format{('custom.tabs.no.results')}
Hi Team,
We are looking for the LIN Protocol Stack for our project with STM32 Controller.
We need LIN protocol stack support for the Bootloader Flash and Controller to act as LIN Slave perform certain operations.
Can you please provide the details and cost?
or
Can we have a LIN module with stack?
Show Less
Dear AURIX Support team,
I'm working now with CCU6 module on TC234 AURIX TriCore chip.
I've used the CCU6_PWM_Capture in Example repository.
Following the example, we will have an ISR Handle that will detect both Rising and Falling edges of an external PWM signal.
I've keep all the configuration as the example, only change the CC6 module. Particularly, the example uses MODULE_CCU60 and CCU60 channel while I use MODULE_CCU61 and CCU61 channel. The other configurations such as channel mode or interrupt1.source I keep the same as example. However, my code detects both Rising and Falling edges at the same time when it calls the ISR handle.
Do you know where is the problem is? Thank you very much
Best regards,
Thien Bui
Show LessHi AURIX support team,
In my old system (using the 16-bits C167 Infineon family chip), it has the Conxtex Pointer feature to change the RAM address .
I would like to implement this feature also in my new Aurix TC234 system. However I cannot find the corresponding part for this feature. Do you have any suggestions?
Best regards,
Thien Bui
Show LessWhere to find the source code of out-of-box demo firmware of KIT_A2G_TC357TA_3V3_TRB?
Thank you.
Hello, I am currently developing the SWAP function of TC397 and have encountered a confusion. I need to consult. As shown in the above figure, can I understand it this way: programming the content of Flash once (updating the App) requires switching between A Bank and B Bank once, and operating UCB once. Therefore, if each TC397 updates the APP by switching between Bank A and Bank B, it can only be updated 400 times? This is obviously not enough, is it because I misunderstood the SWAP limit function?
Show LessHowever I have problems.. about ADC.
I want to read ADC Value.. but i Can't
Result_ADC_Status is 1 (ADC_BUSY)
what should i check?? plz help me..
Adc_SetupResultBuffer(AdcConf_AdcGroup_AdcGroup_Voltage, &Adc_Voltage[0]);
while(1){
Adc_StartGroupConversion(AdcConf_AdcGroup_AdcGroup_Voltage);
Result_ADC_Status = Adc_GetGroupStatus(AdcConf_AdcGroup_AdcGroup_Voltage);
} Show Less
Hi there,
I'm using Memtool 2021 on TriBoard with TC233(DAS) and try to connect to Target but there's a pop up window shows up.
The error message is below.
Message from component "IMTMemtool"
CAN't connect to Target
Message from component "Controller0.Core0. Tc2CoreTarglntf"
CAN't connect target!
Message from component "Controller0.Core0. Tc2CoreTarglntf"
Failed to read target state!
The CPU I am using is "Infineon TC233L".
#DAPminiWiggler
#Memtool
Thank you in advance.
Regards!
Show Less