AURIX™ Forum Discussions
While debugging for 36 service where it communicates via SPI where it is waiting for response from L2.In Lane2 side interrupts is generating for short blk with CRC errors and when I have seen the QSPI status reg error flag(SLSI error) is set. When this SLSI error will set
Show LessHello together,
With kind regards
Philipp
I'm using an AURIX TC377 and need to trigger the ADC on both the rising and falling edge an external discrete input, but after a short delay (~100us). I've looked at using the ECU but that only provides a delay of up to 2us. The CCU6 T12 and T13 look like they could do the job, but couldn't see how to configure them to achieve the desired functionality.
Is the CCU the best approach or is there a better way using the GTM?
Show LessHi,
In order to prepare a MOL (Middle Off Line) test system, we need to add an industrial programmer to in case of UUT firmware is not actualised, update it during the process in this station.
I need the "flash programming specification" of the device these information/documentation need to be detailed for we implement the flash/programming algorithm.
Many Thanks!
José,
Hi Guys,
Is there any available freeRTOS port for Aurix TC399?(Not the demo version) If not, could someone point me to the steps of porting freeRTOS for TC399?
Thanks
Dschunke
Show LessI installed AURIX-v1.9.8Development Studio and selected one of the provided projects -
The project built without any issues. I then setup a debug configuration and it identifies a Generic Infineon AURIX Board with the TC222 . The connection states Universal Debug Access Server with a Host Port / localhost 23.
When I click on Debug, it says Error creating session with the following details:
Error creating session
The debug instrument IO could not be initialized.
The GDI debug instrument provided the following error message.
Could not open Access HW
please help me out
Show LessI need a code related to bootloader in TC375 lite kit.
The Requirement is :
1. Write a simple bootloader that runs the application
2. Write a simple bootloader which is used to load the new application.
Create one Host application that sends the data to the TC375's bootloader.
Add on : Please provide any reference code related to conversion of STM32 code into Aurix TC3xx board.
Show Less
Hi,
Are there any features in the TC299 module that I can use as an RTC?
Hi All, I recently purchased TC387 TFT Board. Looking for LCD demo code which is configured to QSPI0. Provide me some reference project , so that it will be helpful to explore the board.
Show Less